This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

EVMK2H: Program EVMK2H without JTAG Emulator

Prodigy 210 points

Replies: 6

Views: 149

Part Number: EVMK2H

Hi everone,

I receive a EVMK2H board without XDS200 emulator daughtercard. I am new to the EVMK2H board so I try to follow the example from: http://processors.wiki.ti.com/index.php/KeystoneII_Boot_Examples#Ethernet_boot_examples

However, in the example, the JTAG emulator need to be connected to CCS. Any other way I can program EVMK2H board without JTAG emulator? I would be great if the example is provided as well.

Thanks a lot in advance.

  • Hi,

    Sorry, in order to program the evm you need JTAG, see:
       

    Best Regards, 
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Hi Yordan,

    Thank you for your reply.

    May I know if I can get the XDS200 emulator daughtercard from TI, or can I use the external emulator below to replace it:

    http://www.ti.com/tool/TMDSEMU200-U

    Any different between these two emulator?

    Thanks a lot.

  • In reply to Chanh Nguyen64:

    Hi,


    Did you bought the EVM from TI or through distributor? If you bought it from distributor, you should contact them with this request.

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Hi Yordan,

    I am checking on that, but in case I cannot get the XDS200 emulator daughtercard, can I use the below emulator instead?

    http://www.ti.com/tool/TMDSEMU200-U

    Thanks.

  • In reply to Chanh Nguyen64:

    You can use an external emulator with the K2H EVM but  you will need a MIPI60 adapter with 20 pin adapter as indicated by Bill on the E2E here:

    https://e2e.ti.com/support/processors/f/791/p/641392/2367810

    Here is a link to one of the manufacturers who provides the adapter:

    http://www.spectrumdigital.com/14-pin-20pin-cti-jtag-to-mipi-60-jtag-header-adapter/

    Regards,

    Rahul

    --------------------------------------------------------------------------------------------------------------------------------------
    Please click the
    This resolved my issue button on this post if the responses on this E2E thread answers your question.
    --------------------------------------------------------------------------------------------------------------------------------------

     

  • In reply to Rahul Prabhu:

    Hi Rahul,

    Thanks a lot.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.