I am using TMS320DM6441.
I want to use ATA HDD along with CF card. Can these be interfaced simultaneously?
what is maximum size of ATA HDD that can be interfaced with DM6441
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using TMS320DM6441.
I want to use ATA HDD along with CF card. Can these be interfaced simultaneously?
what is maximum size of ATA HDD that can be interfaced with DM6441
Hi,
I am replying this question without consulting the User's Guide. For this reason, please do so.
There are 2 block diagrams that display the interface between a HDD and a CF device. There is a subtle difference between the two. Because of the diffrence in this, I do not think you can use the Master Slave setup where two devices can be hooked up to a single port.
Best regards, Zegeye