Hi.
We have done a custom design based on xam3359zcz. The design of the USB connection is almost identical to that of the Beaglebone. We are using the Ti SDK kernel and those drivers for the MUSB.
Everything seems ok on the hardware side and on the sofware side everything seems to be set up by default as expected in the source code. We are running USB0 as OTG and the USB1 as host. The drivers are loadeded and everything looks ok on the kernel side. But devices are not detected. However we can not get an active signal on the USB_DRVVBUS lines to the boost converter wich is a Ti TPS2505. We presume that this is our problem but we don't see how we can make it USB_DRVVBUS pin active!
Will be very grateful for any help.
Regards
Daniel Eriksson