I was hoping you could clarify the following detail for us, regarding the TMS320VC5506 DSP.
Page 37 of the datasheet discusses the EBSR register. In the diagram showing the position of the bits, it states the initial value for the Parallel Port Mode bits as: “11 if GPIO0 = 0 at reset”. This is the case that we are using, since we are booting from I2C, so GPIO0 must be 0.
The table (page 38) however, lists the value of ‘11’ as “Reserved” for the Parallel Port Mode bits.
Can you please clarify what mode the device will be in at startup in this scenario if we do not write to EBSR? Also, if we later change the value of the other bits in EBSR, should we leave these Parallel Port Mode bits as ‘11’ (this is how they read back), or must they be changed?