Hi
I'm working on OMAPL138_LCDK board and i want to enable USB2.0 OTG on J2 connector. But there is a no initialization part for USB2.0 in board file so my self modified the board file
static __init void omapl138_hawk_usb_init(void)
{
int ret;
u32 cfgchip2;
...
ret = da8xx_register_usb11(&omapl138_hawk_usb11_pdata);
if (ret) {
pr_warning("%s: USB 1.1 registration failed: %d\n",
__func__, ret);
goto usb11_setup_fail;
}
//USB2.0 OTG start
/*
* We have to override VBUS/ID signals when MUSB is configured into the
* host-only mode -- ID pin will float if no cable is connected, so the
* controller won't be able to drive VBUS thinking that it's a B-device.
* Otherwise, we want to use the OTG mode and enable VBUS comparators.
*/
#ifdef CONFIG_USB_MUSB_HOST
cfgchip2 |= CFGCHIP2_FORCE_HOST;
#else
cfgchip2 |= CFGCHIP2_SESENDEN | CFGCHIP2_VBDTCTEN;
#endif
cfgchip2 &= ~CFGCHIP2_OTGMODE;
cfgchip2 |= CFGCHIP2_SESENDEN | CFGCHIP2_VBDTCTEN;
pr_info("USB 2.0 OTG initialization..!!");
ret = davinci_cfg_reg(DA830_USB0_DRVVBUS);
if (ret)
pr_warning("%s: USB 2.0 PinMux setup failed: %d\n",
__func__, ret);
else {
/*
* TPS2065 switch @ 5V supplies 1 A (sustains 1.5 A),
* with the power on to power good time of 3 ms.
*/
ret = da8xx_register_usb20(1000, 3);
if (ret)
pr_warning("%s: USB 2.0 registration failed: %d\n",
__func__, ret);
}
//USB2.0 OTG end
return;
usb11_setup_fail:
gpio_free(DA850_USB1_OC_PIN);
usb11_setup_oc_fail:
gpio_free(DA850_USB1_VBUS_PIN);
}
and configuration file modification is
#
# USB Host Controller Drivers
#
CONFIG_USB_MUSB_HDRC=y
CONFIG_USB_MUSB_DA8XX=y
CONFIG_MUSB_PIO_ONLY=y
#
# USB Miscellaneous drivers
#
CONFIG_USB_GADGET=y
CONFIG_USB_GADGET_VBUS_DRAW=2
CONFIG_USB_GADGET_DUALSPEED=y
#
# OTG and related infrastructure
#
CONFIG_USB_OTG_UTILS=y
# CONFIG_USB_GPIO_VBUS is not set
# CONFIG_USB_ULPI is not set
# CONFIG_NOP_USB_XCEIV is not set
got built success fully and i got this error
da8xx_musb_interrupt 350: VBUS error workaround (delay coming)
da8xx_musb_interrupt 350: VBUS error workaround (delay coming)
root@omapl138-lcdk:/proc/driver# ls
rtc snd-page-alloc
root@omapl138-lcdk:/proc/driver# lsusb
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
there is no node for musb_hrdc.
I dono what i missed and please let me know the issue and how to fix it.
Here i've attached log file and defconfig file.
ARM Clock : 300000000 Hz DDR Clock : 150000000 Hz Net: Ethernet PHY: GENERIC @ 0x07 DaVinci-EMAC Hit any key to stop autoboot: 0 reading boot.scr ** Unable to read "boot.scr" from mmc 0:1 ** reading uImage 2080564 bytes read ## Booting kernel from Legacy Image at c0700000 ... Image Name: Linux-3.1.10 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2080500 Bytes = 2 MiB Load Address: c0008000 Entry Point: c0008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Linux version 3.1.10 (marudham@marudham-desktop) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 PREEMPT Fri Mar 28 17:14 CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177 CPU: VIVT data cache, VIVT instruction cache Machine: AM18x/OMAP-L138 LCDK Memory policy: ECC disabled, Data cache writeback DaVinci da850/omap-l138/am18x variant 0x1 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512 Kernel command line: console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw rootwait ip=off PID hash table entries: 512 (order: -1, 2048 bytes) Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) Memory: 128MB = 128MB total Memory: 125780k/125780k available, 5292k reserved, 0K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xff000000 - 0xffe00000 ( 14 MB) vmalloc : 0xc8800000 - 0xfea00000 ( 866 MB) lowmem : 0xc0000000 - 0xc8000000 ( 128 MB) modules : 0xbf000000 - 0xc0000000 ( 16 MB) .text : 0xc0008000 - 0xc03a6988 (3707 kB) .init : 0xc03a7000 - 0xc03cb000 ( 144 kB) .data : 0xc03cc000 - 0xc03edb00 ( 135 kB) .bss : 0xc03edb24 - 0xc04075fc ( 103 kB) SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Preemptible hierarchical RCU implementation. NR_IRQS:245 Console: colour dummy device 80x30 Calibrating delay loop... 148.88 BogoMIPS (lpj=744448) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok DaVinci: 144 gpio irqs NET: Registered protocol family 16 EMAC: MII PHY configured USB 2.0 OTG initialization..!! preapring LED initializing gpio_led configured the pin mux for gpio led..>>>>> FPC1080 init >>>> configured the pin mux for FPC gpio ..>>>>> Initiated FPC1080 successfull..!! bio: create slab <bio-0> at 0 SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb Advanced Linux Sound Architecture Driver Version 1.0.24. Switching to clocksource timer0_1 Switched to NOHz mode on CPU #0 musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) Waiting for USB PHY clock good... musb-hdrc musb-hdrc: MUSB HDRC host driver musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1 usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb1: Product: MUSB HDRC host driver usb usb1: Manufacturer: Linux 3.1.10 musb-hcd usb usb1: SerialNumber: musb-hdrc hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected musb-hdrc musb-hdrc: USB OTG mode controller at fee00000 using PIO, IRQ 58 NET: Registered protocol family 2 IP route cache hash table entries: 1024 (order: 0, 4096 bytes) TCP established hash table entries: 4096 (order: 3, 32768 bytes) TCP bind hash table entries: 4096 (order: 2, 16384 bytes) TCP: Hash tables configured (established 4096 bind 4096) TCP reno registered UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. msgmni has been set to 245 io scheduler noop registered (default) da8xx_lcdc da8xx_lcdc.0: GLCD: Found VGA_Monitor panel da8xx_musb_interrupt 350: VBUS error workaround (delay coming) Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A console [ttyS2] enabled brd: module loaded ahci ahci: forcing PORTS_IMPL to 0x1 ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc scsi0 : ahci_platform ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67 spi_davinci spi_davinci.1: DMA: supported spi_davinci spi_davinci.1: DMA: RX channel: 18, TX channel: 19, event queue: 0 spi_davinci spi_davinci.1: Controller at 0xfef0e000 davinci_mdio davinci_mdio.0: davinci mdio revision 1.5 davinci_mdio davinci_mdio.0: detected phy mask ffffff7f davinci_mdio.0: probed davinci_mdio davinci_mdio.0: phy[7]: device 0:07, driver unknown ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver ohci ohci.0: DA8xx OHCI ohci ohci.0: new USB bus registered, assigned bus number 2 Waiting for USB PHY clock good... ohci ohci.0: irq 59, io mem 0x01e25000 usb usb2: New USB device found, idVendor=1d6b, idProduct=0001 usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb2: Product: DA8xx OHCI usb usb2: Manufacturer: Linux 3.1.10 ohci_hcd usb usb2: SerialNumber: ohci.0 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 omap_rtc: RTC power up reset detected omap_rtc: already running i2c /dev entries driver davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode ALSA device list: No soundcards found. TCP cubic registered NET: Registered protocol family 17 davinci_emac davinci_emac.1: using random MAC addr: e6:cf:f3:c7:50:1b console [netcon0] enabled netconsole: network logging started omap_rtc omap_rtc: setting system clock to 2012-04-11 08:32:02 UTC (1334133122) mmc0: new SD card at address 1234 mmcblk0: mmc0:1234 SA02G 1.83 GiB mmcblk0: p1 p2 ata1: SATA link down (SStatus 0 SControl 300) kjournald starting. Commit interval 5 seconds EXT3-fs (mmcblk0p2): using internal journal EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode VFS: Mounted root (ext3 filesystem) on device 179:2. Freeing init memory: 144K INIT: da8xx_musb_interrupt 350: VBUS error workaround (delay coming) version 2.86 booting Please wait: booting... Starting udev udevd (965): /proc/965/oom_adj is deprecated, please use /proc/965/oom_score_adj instead. da8xx_musb_interrupt 350: VBUS error workaround (delay coming) da8xx_musb_interrupt 350: VBUS error workaround (delay coming) Remounting root file system... Caching udev devnodes Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory NET: Registered protocol family 10 ALSA: Restoring mixer settings... Configuring network interfaces... ifup: misplaced option " pre-up" done. /usr/sbin/alsactl: load_state:1625: No soundcards found... Setting up IP spoofing protection: rp_filter. INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Hardware abstraction layer hald Starting Dropbear SSH server: dropbear. Starting telnet daemon. Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting Lighttpd Web Server: lighttpd. 2012-04-11 08:32:40: (log.c.166) server started / Starting Matrix GUI applicationdavinci_mdio davinci_mdio.0: resetting idled controller net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:07, id=7c0f1) ADDRCONF(NETDEV_UP): eth0: link is not ready
# # Automatically generated file; DO NOT EDIT. # Linux/arm 3.1.10 Kernel Configuration # CONFIG_ARM=y CONFIG_SYS_SUPPORTS_APM_EMULATION=y CONFIG_GENERIC_GPIO=y # CONFIG_ARCH_USES_GETTIMEOFFSET is not set CONFIG_GENERIC_CLOCKEVENTS=y CONFIG_KTIME_SCALAR=y CONFIG_HAVE_PROC_CPU=y CONFIG_STACKTRACE_SUPPORT=y CONFIG_HAVE_LATENCYTOP_SUPPORT=y CONFIG_LOCKDEP_SUPPORT=y CONFIG_TRACE_IRQFLAGS_SUPPORT=y CONFIG_HARDIRQS_SW_RESEND=y CONFIG_GENERIC_IRQ_PROBE=y CONFIG_RWSEM_GENERIC_SPINLOCK=y CONFIG_ARCH_HAS_CPUFREQ=y CONFIG_ARCH_HAS_CPU_IDLE_WAIT=y CONFIG_GENERIC_HWEIGHT=y CONFIG_GENERIC_CALIBRATE_DELAY=y CONFIG_ZONE_DMA=y CONFIG_NEED_DMA_MAP_STATE=y CONFIG_VECTORS_BASE=0xffff0000 # CONFIG_ARM_PATCH_PHYS_VIRT is not set CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config" CONFIG_HAVE_IRQ_WORK=y # # General setup # CONFIG_EXPERIMENTAL=y CONFIG_BROKEN_ON_SMP=y CONFIG_INIT_ENV_ARG_LIMIT=32 CONFIG_CROSS_COMPILE="" CONFIG_LOCALVERSION="" CONFIG_LOCALVERSION_AUTO=y CONFIG_HAVE_KERNEL_GZIP=y CONFIG_HAVE_KERNEL_LZMA=y CONFIG_HAVE_KERNEL_LZO=y CONFIG_KERNEL_GZIP=y # CONFIG_KERNEL_LZMA is not set # CONFIG_KERNEL_LZO is not set CONFIG_DEFAULT_HOSTNAME="(none)" # CONFIG_SWAP is not set CONFIG_SYSVIPC=y CONFIG_SYSVIPC_SYSCTL=y CONFIG_POSIX_MQUEUE=y CONFIG_POSIX_MQUEUE_SYSCTL=y # CONFIG_BSD_PROCESS_ACCT is not set # CONFIG_FHANDLE is not set # CONFIG_TASKSTATS is not set # CONFIG_AUDIT is not set CONFIG_HAVE_GENERIC_HARDIRQS=y # # IRQ subsystem # CONFIG_GENERIC_HARDIRQS=y CONFIG_HAVE_SPARSE_IRQ=y CONFIG_GENERIC_IRQ_SHOW=y CONFIG_GENERIC_IRQ_CHIP=y # CONFIG_SPARSE_IRQ is not set # # RCU Subsystem # CONFIG_TREE_PREEMPT_RCU=y # CONFIG_TINY_RCU is not set # CONFIG_TINY_PREEMPT_RCU is not set CONFIG_PREEMPT_RCU=y # CONFIG_RCU_TRACE is not set CONFIG_RCU_FANOUT=32 # CONFIG_RCU_FANOUT_EXACT is not set # CONFIG_TREE_RCU_TRACE is not set # CONFIG_RCU_BOOST is not set CONFIG_IKCONFIG=y CONFIG_IKCONFIG_PROC=y CONFIG_LOG_BUF_SHIFT=14 # CONFIG_CGROUPS is not set # CONFIG_NAMESPACES is not set # CONFIG_SCHED_AUTOGROUP is not set # CONFIG_SYSFS_DEPRECATED is not set # CONFIG_RELAY is not set CONFIG_BLK_DEV_INITRD=y CONFIG_INITRAMFS_SOURCE="" CONFIG_RD_GZIP=y # CONFIG_RD_BZIP2 is not set # CONFIG_RD_LZMA is not set # CONFIG_RD_XZ is not set # CONFIG_RD_LZO is not set # CONFIG_CC_OPTIMIZE_FOR_SIZE is not set CONFIG_SYSCTL=y CONFIG_ANON_INODES=y CONFIG_EXPERT=y CONFIG_UID16=y CONFIG_SYSCTL_SYSCALL=y CONFIG_KALLSYMS=y # CONFIG_KALLSYMS_ALL is not set CONFIG_HOTPLUG=y CONFIG_PRINTK=y CONFIG_BUG=y CONFIG_ELF_CORE=y CONFIG_BASE_FULL=y CONFIG_FUTEX=y CONFIG_EPOLL=y CONFIG_SIGNALFD=y CONFIG_TIMERFD=y CONFIG_EVENTFD=y CONFIG_SHMEM=y CONFIG_AIO=y # CONFIG_EMBEDDED is not set CONFIG_HAVE_PERF_EVENTS=y CONFIG_PERF_USE_VMALLOC=y # # Kernel Performance Events And Counters # # CONFIG_PERF_EVENTS is not set # CONFIG_PERF_COUNTERS is not set CONFIG_VM_EVENT_COUNTERS=y CONFIG_SLUB_DEBUG=y CONFIG_COMPAT_BRK=y # CONFIG_SLAB is not set CONFIG_SLUB=y # CONFIG_SLOB is not set # CONFIG_PROFILING is not set CONFIG_HAVE_OPROFILE=y # CONFIG_KPROBES is not set CONFIG_HAVE_KPROBES=y CONFIG_HAVE_KRETPROBES=y CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y CONFIG_HAVE_CLK=y CONFIG_HAVE_DMA_API_DEBUG=y # # GCOV-based kernel profiling # CONFIG_HAVE_GENERIC_DMA_COHERENT=y CONFIG_SLABINFO=y CONFIG_RT_MUTEXES=y CONFIG_BASE_SMALL=0 CONFIG_MODULES=y # CONFIG_MODULE_FORCE_LOAD is not set CONFIG_MODULE_UNLOAD=y CONFIG_MODULE_FORCE_UNLOAD=y CONFIG_MODVERSIONS=y # CONFIG_MODULE_SRCVERSION_ALL is not set CONFIG_BLOCK=y CONFIG_LBDAF=y # CONFIG_BLK_DEV_BSG is not set # CONFIG_BLK_DEV_BSGLIB is not set # CONFIG_BLK_DEV_INTEGRITY is not set # # IO Schedulers # CONFIG_IOSCHED_NOOP=y # CONFIG_IOSCHED_DEADLINE is not set # CONFIG_IOSCHED_CFQ is not set CONFIG_DEFAULT_NOOP=y CONFIG_DEFAULT_IOSCHED="noop" # CONFIG_INLINE_SPIN_TRYLOCK is not set # CONFIG_INLINE_SPIN_TRYLOCK_BH is not set # CONFIG_INLINE_SPIN_LOCK is not set # CONFIG_INLINE_SPIN_LOCK_BH is not set # CONFIG_INLINE_SPIN_LOCK_IRQ is not set # CONFIG_INLINE_SPIN_LOCK_IRQSAVE is not set # CONFIG_INLINE_SPIN_UNLOCK is not set # CONFIG_INLINE_SPIN_UNLOCK_BH is not set # CONFIG_INLINE_SPIN_UNLOCK_IRQ is not set # CONFIG_INLINE_SPIN_UNLOCK_IRQRESTORE is not set # CONFIG_INLINE_READ_TRYLOCK is not set # CONFIG_INLINE_READ_LOCK is not set # CONFIG_INLINE_READ_LOCK_BH is not set # CONFIG_INLINE_READ_LOCK_IRQ is not set # CONFIG_INLINE_READ_LOCK_IRQSAVE is not set # CONFIG_INLINE_READ_UNLOCK is not set # CONFIG_INLINE_READ_UNLOCK_BH is not set # CONFIG_INLINE_READ_UNLOCK_IRQ is not set # CONFIG_INLINE_READ_UNLOCK_IRQRESTORE is not set # CONFIG_INLINE_WRITE_TRYLOCK is not set # CONFIG_INLINE_WRITE_LOCK is not set # CONFIG_INLINE_WRITE_LOCK_BH is not set # CONFIG_INLINE_WRITE_LOCK_IRQ is not set # CONFIG_INLINE_WRITE_LOCK_IRQSAVE is not set # CONFIG_INLINE_WRITE_UNLOCK is not set # CONFIG_INLINE_WRITE_UNLOCK_BH is not set # CONFIG_INLINE_WRITE_UNLOCK_IRQ is not set # CONFIG_INLINE_WRITE_UNLOCK_IRQRESTORE is not set # CONFIG_MUTEX_SPIN_ON_OWNER is not set # CONFIG_FREEZER is not set # # System Type # CONFIG_MMU=y # CONFIG_ARCH_INTEGRATOR is not set # CONFIG_ARCH_REALVIEW is not set # CONFIG_ARCH_VERSATILE is not set # CONFIG_ARCH_VEXPRESS is not set # CONFIG_ARCH_AT91 is not set # CONFIG_ARCH_BCMRING is not set # CONFIG_ARCH_CLPS711X is not set # CONFIG_ARCH_CNS3XXX is not set # CONFIG_ARCH_GEMINI is not set # CONFIG_ARCH_PRIMA2 is not set # CONFIG_ARCH_EBSA110 is not set # CONFIG_ARCH_EP93XX is not set # CONFIG_ARCH_FOOTBRIDGE is not set # CONFIG_ARCH_MXC is not set # CONFIG_ARCH_MXS is not set # CONFIG_ARCH_NETX is not set # CONFIG_ARCH_H720X is not set # CONFIG_ARCH_IOP13XX is not set # CONFIG_ARCH_IOP32X is not set # CONFIG_ARCH_IOP33X is not set # CONFIG_ARCH_IXP23XX is not set # CONFIG_ARCH_IXP2000 is not set # CONFIG_ARCH_IXP4XX is not set # CONFIG_ARCH_DOVE is not set # CONFIG_ARCH_KIRKWOOD is not set # CONFIG_ARCH_LPC32XX is not set # CONFIG_ARCH_MV78XX0 is not set # CONFIG_ARCH_ORION5X is not set # CONFIG_ARCH_MMP is not set # CONFIG_ARCH_KS8695 is not set # CONFIG_ARCH_W90X900 is not set # CONFIG_ARCH_NUC93X is not set # CONFIG_ARCH_TEGRA is not set # CONFIG_ARCH_PNX4008 is not set # CONFIG_ARCH_PXA is not set # CONFIG_ARCH_MSM is not set # CONFIG_ARCH_SHMOBILE is not set # CONFIG_ARCH_RPC is not set # CONFIG_ARCH_SA1100 is not set # CONFIG_ARCH_S3C2410 is not set # CONFIG_ARCH_S3C64XX is not set # CONFIG_ARCH_S5P64X0 is not set # CONFIG_ARCH_S5PC100 is not set # CONFIG_ARCH_S5PV210 is not set # CONFIG_ARCH_EXYNOS4 is not set # CONFIG_ARCH_SHARK is not set # CONFIG_ARCH_TCC_926 is not set # CONFIG_ARCH_U300 is not set # CONFIG_ARCH_U8500 is not set # CONFIG_ARCH_NOMADIK is not set CONFIG_ARCH_DAVINCI=y # CONFIG_ARCH_OMAP is not set # CONFIG_PLAT_SPEAR is not set # CONFIG_ARCH_VT8500 is not set # CONFIG_ARCH_ZYNQ is not set CONFIG_CP_INTC=y # # TI DaVinci Implementations # # # DaVinci Core Type # # CONFIG_ARCH_DAVINCI_DM644x is not set # CONFIG_ARCH_DAVINCI_DM355 is not set # CONFIG_ARCH_DAVINCI_DM646x is not set # CONFIG_ARCH_DAVINCI_DA830 is not set CONFIG_ARCH_DAVINCI_DA850=y CONFIG_ARCH_DAVINCI_DA8XX=y # CONFIG_ARCH_DAVINCI_DM365 is not set # CONFIG_ARCH_DAVINCI_TNETV107X is not set # # DaVinci Board Type # # CONFIG_MACH_DAVINCI_DA850_EVM is not set CONFIG_GPIO_PCA953X=y CONFIG_KEYBOARD_GPIO_POLLED=y # CONFIG_MACH_MITYOMAPL138 is not set CONFIG_MACH_OMAPL138_HAWKBOARD=y CONFIG_HAWKBOARD_LCDK=y # CONFIG_HAWKBOARD_ORIGINAL is not set CONFIG_DAVINCI_MUX=y # CONFIG_DAVINCI_MUX_DEBUG is not set # CONFIG_DAVINCI_MUX_WARNINGS is not set CONFIG_DAVINCI_RESET_CLOCKS=y # # System MMU # # # Processor Type # CONFIG_CPU_ARM926T=y CONFIG_CPU_32v5=y CONFIG_CPU_ABRT_EV5TJ=y CONFIG_CPU_PABRT_LEGACY=y CONFIG_CPU_CACHE_VIVT=y CONFIG_CPU_COPY_V4WB=y CONFIG_CPU_TLB_V4WBI=y CONFIG_CPU_CP15=y CONFIG_CPU_CP15_MMU=y CONFIG_CPU_USE_DOMAINS=y # # Processor Features # CONFIG_ARM_THUMB=y # CONFIG_CPU_ICACHE_DISABLE is not set # CONFIG_CPU_DCACHE_DISABLE is not set # CONFIG_CPU_DCACHE_WRITETHROUGH is not set # CONFIG_CPU_CACHE_ROUND_ROBIN is not set CONFIG_ARM_L1_CACHE_SHIFT=5 # # Bus support # # CONFIG_PCI_SYSCALL is not set # CONFIG_ARCH_SUPPORTS_MSI is not set # CONFIG_PCCARD is not set # # Kernel Features # CONFIG_TICK_ONESHOT=y CONFIG_NO_HZ=y CONFIG_HIGH_RES_TIMERS=y CONFIG_GENERIC_CLOCKEVENTS_BUILD=y CONFIG_VMSPLIT_3G=y # CONFIG_VMSPLIT_2G is not set # CONFIG_VMSPLIT_1G is not set CONFIG_PAGE_OFFSET=0xC0000000 # CONFIG_PREEMPT_NONE is not set # CONFIG_PREEMPT_VOLUNTARY is not set CONFIG_PREEMPT=y CONFIG_PREEMPT_COUNT=y CONFIG_HZ=100 CONFIG_AEABI=y # CONFIG_OABI_COMPAT is not set CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y # CONFIG_ARCH_SPARSEMEM_DEFAULT is not set # CONFIG_ARCH_SELECT_MEMORY_MODEL is not set CONFIG_HAVE_ARCH_PFN_VALID=y # CONFIG_HIGHMEM is not set CONFIG_SELECT_MEMORY_MODEL=y CONFIG_FLATMEM_MANUAL=y CONFIG_FLATMEM=y CONFIG_FLAT_NODE_MEM_MAP=y CONFIG_HAVE_MEMBLOCK=y CONFIG_PAGEFLAGS_EXTENDED=y CONFIG_SPLIT_PTLOCK_CPUS=999999 # CONFIG_COMPACTION is not set # CONFIG_PHYS_ADDR_T_64BIT is not set CONFIG_ZONE_DMA_FLAG=1 CONFIG_BOUNCE=y CONFIG_VIRT_TO_BUS=y # CONFIG_KSM is not set CONFIG_DEFAULT_MMAP_MIN_ADDR=4096 CONFIG_NEED_PER_CPU_KM=y # CONFIG_CLEANCACHE is not set CONFIG_FORCE_MAX_ZONEORDER=11 # CONFIG_LEDS is not set CONFIG_ALIGNMENT_TRAP=y # CONFIG_UACCESS_WITH_MEMCPY is not set # CONFIG_SECCOMP is not set # CONFIG_CC_STACKPROTECTOR is not set # CONFIG_DEPRECATED_PARAM_STRUCT is not set # # Boot options # # CONFIG_USE_OF is not set CONFIG_ZBOOT_ROM_TEXT=0x0 CONFIG_ZBOOT_ROM_BSS=0x0 CONFIG_CMDLINE="" # CONFIG_XIP_KERNEL is not set # CONFIG_KEXEC is not set # CONFIG_CRASH_DUMP is not set # CONFIG_AUTO_ZRELADDR is not set # # CPU Power Management # # # CPU Frequency scaling # CONFIG_CPU_FREQ=y CONFIG_CPU_FREQ_TABLE=y CONFIG_CPU_FREQ_STAT=y # CONFIG_CPU_FREQ_STAT_DETAILS is not set # CONFIG_CPU_FREQ_DEFAULT_GOV_PERFORMANCE is not set # CONFIG_CPU_FREQ_DEFAULT_GOV_POWERSAVE is not set CONFIG_CPU_FREQ_DEFAULT_GOV_USERSPACE=y # CONFIG_CPU_FREQ_DEFAULT_GOV_ONDEMAND is not set # CONFIG_CPU_FREQ_DEFAULT_GOV_CONSERVATIVE is not set CONFIG_CPU_FREQ_GOV_PERFORMANCE=m CONFIG_CPU_FREQ_GOV_POWERSAVE=m CONFIG_CPU_FREQ_GOV_USERSPACE=y CONFIG_CPU_FREQ_GOV_ONDEMAND=m # CONFIG_CPU_FREQ_GOV_CONSERVATIVE is not set # # ARM CPU frequency scaling drivers # # CONFIG_CPU_IDLE is not set # # Floating point emulation # # # At least one emulation must be selected # # CONFIG_VFP is not set # # Userspace binary formats # CONFIG_BINFMT_ELF=y CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS=y CONFIG_HAVE_AOUT=y # CONFIG_BINFMT_AOUT is not set # CONFIG_BINFMT_MISC is not set # # Power management options # # CONFIG_SUSPEND is not set # CONFIG_PM_RUNTIME is not set CONFIG_ARCH_SUSPEND_POSSIBLE=y CONFIG_NET=y # # Networking options # CONFIG_PACKET=y CONFIG_UNIX=y CONFIG_XFRM=y # CONFIG_XFRM_USER is not set # CONFIG_XFRM_SUB_POLICY is not set # CONFIG_XFRM_MIGRATE is not set # CONFIG_XFRM_STATISTICS is not set # CONFIG_NET_KEY is not set CONFIG_INET=y # CONFIG_IP_MULTICAST is not set # CONFIG_IP_ADVANCED_ROUTER is not set CONFIG_IP_PNP=y CONFIG_IP_PNP_DHCP=y # CONFIG_IP_PNP_BOOTP is not set # CONFIG_IP_PNP_RARP is not set # CONFIG_NET_IPIP is not set # CONFIG_NET_IPGRE_DEMUX is not set # CONFIG_ARPD is not set # CONFIG_SYN_COOKIES is not set # CONFIG_INET_AH is not set # CONFIG_INET_ESP is not set # CONFIG_INET_IPCOMP is not set # CONFIG_INET_XFRM_TUNNEL is not set CONFIG_INET_TUNNEL=m CONFIG_INET_XFRM_MODE_TRANSPORT=y CONFIG_INET_XFRM_MODE_TUNNEL=y CONFIG_INET_XFRM_MODE_BEET=y # CONFIG_INET_LRO is not set CONFIG_INET_DIAG=y CONFIG_INET_TCP_DIAG=y # CONFIG_TCP_CONG_ADVANCED is not set CONFIG_TCP_CONG_CUBIC=y CONFIG_DEFAULT_TCP_CONG="cubic" # CONFIG_TCP_MD5SIG is not set CONFIG_IPV6=m # CONFIG_IPV6_PRIVACY is not set # CONFIG_IPV6_ROUTER_PREF is not set # CONFIG_IPV6_OPTIMISTIC_DAD is not set # CONFIG_INET6_AH is not set # CONFIG_INET6_ESP is not set # CONFIG_INET6_IPCOMP is not set # CONFIG_IPV6_MIP6 is not set # CONFIG_INET6_XFRM_TUNNEL is not set # CONFIG_INET6_TUNNEL is not set CONFIG_INET6_XFRM_MODE_TRANSPORT=m CONFIG_INET6_XFRM_MODE_TUNNEL=m CONFIG_INET6_XFRM_MODE_BEET=m # CONFIG_INET6_XFRM_MODE_ROUTEOPTIMIZATION is not set CONFIG_IPV6_SIT=m # CONFIG_IPV6_SIT_6RD is not set CONFIG_IPV6_NDISC_NODETYPE=y # CONFIG_IPV6_TUNNEL is not set # CONFIG_IPV6_MULTIPLE_TABLES is not set # CONFIG_IPV6_MROUTE is not set # CONFIG_NETWORK_SECMARK is not set # CONFIG_NETWORK_PHY_TIMESTAMPING is not set CONFIG_NETFILTER=y # CONFIG_NETFILTER_DEBUG is not set CONFIG_NETFILTER_ADVANCED=y # # Core Netfilter Configuration # # CONFIG_NETFILTER_NETLINK_QUEUE is not set # CONFIG_NETFILTER_NETLINK_LOG is not set # CONFIG_NF_CONNTRACK is not set # CONFIG_NETFILTER_XTABLES is not set # CONFIG_IP_VS is not set # # IP: Netfilter Configuration # # CONFIG_NF_DEFRAG_IPV4 is not set # CONFIG_IP_NF_QUEUE is not set # CONFIG_IP_NF_IPTABLES is not set # CONFIG_IP_NF_ARPTABLES is not set # # IPv6: Netfilter Configuration # # CONFIG_NF_DEFRAG_IPV6 is not set # CONFIG_IP6_NF_QUEUE is not set # CONFIG_IP6_NF_IPTABLES is not set # CONFIG_IP_DCCP is not set # CONFIG_IP_SCTP is not set # CONFIG_RDS is not set # CONFIG_TIPC is not set # CONFIG_ATM is not set # CONFIG_L2TP is not set # CONFIG_BRIDGE is not set # CONFIG_NET_DSA is not set # CONFIG_VLAN_8021Q is not set # CONFIG_DECNET is not set # CONFIG_LLC2 is not set # CONFIG_IPX is not set # CONFIG_ATALK is not set # CONFIG_X25 is not set # CONFIG_LAPB is not set # CONFIG_ECONET is not set # CONFIG_WAN_ROUTER is not set # CONFIG_PHONET is not set # CONFIG_IEEE802154 is not set # CONFIG_NET_SCHED is not set # CONFIG_DCB is not set # CONFIG_BATMAN_ADV is not set # # Network testing # # CONFIG_NET_PKTGEN is not set # CONFIG_HAMRADIO is not set # CONFIG_CAN is not set # CONFIG_IRDA is not set # CONFIG_BT is not set # CONFIG_AF_RXRPC is not set CONFIG_WIRELESS=y # CONFIG_CFG80211 is not set # CONFIG_LIB80211 is not set # # CFG80211 needs to be enabled for MAC80211 # # CONFIG_WIMAX is not set # CONFIG_RFKILL is not set # CONFIG_NET_9P is not set # CONFIG_CAIF is not set # CONFIG_CEPH_LIB is not set # CONFIG_NFC is not set # # Device Drivers # # # Generic Driver Options # CONFIG_UEVENT_HELPER_PATH="/sbin/hotplug" # CONFIG_DEVTMPFS is not set CONFIG_STANDALONE=y CONFIG_PREVENT_FIRMWARE_BUILD=y # CONFIG_FW_LOADER is not set # CONFIG_DEBUG_DRIVER is not set # CONFIG_DEBUG_DEVRES is not set # CONFIG_SYS_HYPERVISOR is not set # CONFIG_CONNECTOR is not set # CONFIG_MTD is not set # CONFIG_PARPORT is not set CONFIG_BLK_DEV=y # CONFIG_BLK_DEV_COW_COMMON is not set CONFIG_BLK_DEV_LOOP=m CONFIG_BLK_DEV_LOOP_MIN_COUNT=8 # CONFIG_BLK_DEV_CRYPTOLOOP is not set # # DRBD disabled because PROC_FS, INET or CONNECTOR not selected # # CONFIG_BLK_DEV_NBD is not set # CONFIG_BLK_DEV_UB is not set CONFIG_BLK_DEV_RAM=y CONFIG_BLK_DEV_RAM_COUNT=1 CONFIG_BLK_DEV_RAM_SIZE=32768 # CONFIG_BLK_DEV_XIP is not set # CONFIG_CDROM_PKTCDVD is not set # CONFIG_ATA_OVER_ETH is not set # CONFIG_MG_DISK is not set # CONFIG_BLK_DEV_RBD is not set # CONFIG_SENSORS_LIS3LV02D is not set # CONFIG_MISC_DEVICES is not set CONFIG_HAVE_IDE=y # CONFIG_IDE is not set # # SCSI device support # CONFIG_SCSI_MOD=y # CONFIG_RAID_ATTRS is not set CONFIG_SCSI=y CONFIG_SCSI_DMA=y # CONFIG_SCSI_TGT is not set # CONFIG_SCSI_NETLINK is not set CONFIG_SCSI_PROC_FS=y # # SCSI support type (disk, tape, CD-ROM) # CONFIG_BLK_DEV_SD=m # CONFIG_CHR_DEV_ST is not set # CONFIG_CHR_DEV_OSST is not set # CONFIG_BLK_DEV_SR is not set # CONFIG_CHR_DEV_SG is not set # CONFIG_CHR_DEV_SCH is not set # CONFIG_SCSI_MULTI_LUN is not set # CONFIG_SCSI_CONSTANTS is not set # CONFIG_SCSI_LOGGING is not set # CONFIG_SCSI_SCAN_ASYNC is not set CONFIG_SCSI_WAIT_SCAN=m # # SCSI Transports # # CONFIG_SCSI_SPI_ATTRS is not set # CONFIG_SCSI_FC_ATTRS is not set # CONFIG_SCSI_ISCSI_ATTRS is not set # CONFIG_SCSI_SAS_ATTRS is not set # CONFIG_SCSI_SAS_LIBSAS is not set # CONFIG_SCSI_SRP_ATTRS is not set CONFIG_SCSI_LOWLEVEL=y # CONFIG_ISCSI_TCP is not set # CONFIG_ISCSI_BOOT_SYSFS is not set # CONFIG_LIBFC is not set # CONFIG_LIBFCOE is not set # CONFIG_SCSI_DEBUG is not set # CONFIG_SCSI_DH is not set # CONFIG_SCSI_OSD_INITIATOR is not set CONFIG_ATA=y # CONFIG_ATA_NONSTANDARD is not set CONFIG_ATA_VERBOSE_ERROR=y CONFIG_SATA_PMP=y # # Controllers with non-SFF native interface # CONFIG_SATA_AHCI_PLATFORM=y CONFIG_ATA_SFF=y # # SFF controllers with custom DMA interface # CONFIG_ATA_BMDMA=y # # SATA SFF controllers with BMDMA # # CONFIG_SATA_MV is not set # # PATA SFF controllers with BMDMA # # # PIO-only SFF controllers # # CONFIG_PATA_PLATFORM is not set # # Generic fallback / legacy drivers # # CONFIG_MD is not set # CONFIG_TARGET_CORE is not set CONFIG_NETDEVICES=y # CONFIG_DUMMY is not set # CONFIG_BONDING is not set # CONFIG_MACVLAN is not set # CONFIG_EQUALIZER is not set CONFIG_TUN=m # CONFIG_VETH is not set CONFIG_MII=y CONFIG_PHYLIB=y # # MII PHY device drivers # # CONFIG_MARVELL_PHY is not set # CONFIG_DAVICOM_PHY is not set # CONFIG_QSEMI_PHY is not set CONFIG_LXT_PHY=y # CONFIG_CICADA_PHY is not set # CONFIG_VITESSE_PHY is not set # CONFIG_SMSC_PHY is not set # CONFIG_BROADCOM_PHY is not set # CONFIG_ICPLUS_PHY is not set # CONFIG_REALTEK_PHY is not set # CONFIG_NATIONAL_PHY is not set # CONFIG_STE10XP is not set CONFIG_LSI_ET1011C_PHY=y # CONFIG_MICREL_PHY is not set # CONFIG_FIXED_PHY is not set # CONFIG_MDIO_BITBANG is not set CONFIG_NET_ETHERNET=y # CONFIG_AX88796 is not set # CONFIG_SMC91X is not set CONFIG_TI_DAVINCI_EMAC=y CONFIG_TI_DAVINCI_MDIO=y CONFIG_TI_DAVINCI_CPDMA=y # CONFIG_DM9000 is not set # CONFIG_ETHOC is not set # CONFIG_SMC911X is not set # CONFIG_SMSC911X is not set # CONFIG_DNET is not set # CONFIG_IBM_NEW_EMAC_ZMII is not set # CONFIG_IBM_NEW_EMAC_RGMII is not set # CONFIG_IBM_NEW_EMAC_TAH is not set # CONFIG_IBM_NEW_EMAC_EMAC4 is not set # CONFIG_IBM_NEW_EMAC_NO_FLOW_CTRL is not set # CONFIG_IBM_NEW_EMAC_MAL_CLR_ICINTSTAT is not set # CONFIG_IBM_NEW_EMAC_MAL_COMMON_ERR is not set # CONFIG_B44 is not set # CONFIG_KS8851_MLL is not set # CONFIG_FTMAC100 is not set # CONFIG_NETDEV_1000 is not set # CONFIG_NETDEV_10000 is not set # CONFIG_WLAN is not set # # Enable WiMAX (Networking options) to see the WiMAX drivers # # # USB Network Adapters # # CONFIG_USB_CATC is not set # CONFIG_USB_KAWETH is not set # CONFIG_USB_PEGASUS is not set # CONFIG_USB_RTL8150 is not set # CONFIG_USB_USBNET is not set # CONFIG_USB_IPHETH is not set # CONFIG_WAN is not set # # CAIF transport drivers # # CONFIG_PPP is not set # CONFIG_SLIP is not set CONFIG_NETCONSOLE=y CONFIG_NETPOLL=y CONFIG_NETPOLL_TRAP=y CONFIG_NET_POLL_CONTROLLER=y # CONFIG_ISDN is not set # CONFIG_PHONE is not set # # Input device support # CONFIG_INPUT=y # CONFIG_INPUT_FF_MEMLESS is not set CONFIG_INPUT_POLLDEV=y # CONFIG_INPUT_SPARSEKMAP is not set # # Userland interfaces # CONFIG_INPUT_MOUSEDEV=m CONFIG_INPUT_MOUSEDEV_PSAUX=y CONFIG_INPUT_MOUSEDEV_SCREEN_X=1024 CONFIG_INPUT_MOUSEDEV_SCREEN_Y=768 # CONFIG_INPUT_JOYDEV is not set CONFIG_INPUT_EVDEV=m CONFIG_INPUT_EVBUG=m # # Input Device Drivers # CONFIG_INPUT_KEYBOARD=y # CONFIG_KEYBOARD_ADP5588 is not set # CONFIG_KEYBOARD_ADP5589 is not set CONFIG_KEYBOARD_ATKBD=m # CONFIG_KEYBOARD_QT1070 is not set # CONFIG_KEYBOARD_QT2160 is not set # CONFIG_KEYBOARD_LKKBD is not set CONFIG_KEYBOARD_GPIO=y # CONFIG_KEYBOARD_TCA6416 is not set # CONFIG_KEYBOARD_MATRIX is not set # CONFIG_KEYBOARD_MAX7359 is not set # CONFIG_KEYBOARD_MCS is not set # CONFIG_KEYBOARD_MPR121 is not set # CONFIG_KEYBOARD_NEWTON is not set # CONFIG_KEYBOARD_OPENCORES is not set # CONFIG_KEYBOARD_STOWAWAY is not set # CONFIG_KEYBOARD_SUNKBD is not set CONFIG_KEYBOARD_XTKBD=m # CONFIG_INPUT_MOUSE is not set # CONFIG_INPUT_JOYSTICK is not set # CONFIG_INPUT_TABLET is not set CONFIG_INPUT_TOUCHSCREEN=y # CONFIG_TOUCHSCREEN_AD7879 is not set # CONFIG_TOUCHSCREEN_ATMEL_MXT is not set # CONFIG_TOUCHSCREEN_BU21013 is not set # CONFIG_TOUCHSCREEN_CY8CTMG110 is not set # CONFIG_TOUCHSCREEN_DYNAPRO is not set # CONFIG_TOUCHSCREEN_HAMPSHIRE is not set # CONFIG_TOUCHSCREEN_EETI is not set # CONFIG_TOUCHSCREEN_FUJITSU is not set # CONFIG_TOUCHSCREEN_GUNZE is not set # CONFIG_TOUCHSCREEN_ELO is not set # CONFIG_TOUCHSCREEN_WACOM_W8001 is not set # CONFIG_TOUCHSCREEN_MAX11801 is not set # CONFIG_TOUCHSCREEN_MCS5000 is not set # CONFIG_TOUCHSCREEN_MTOUCH is not set # CONFIG_TOUCHSCREEN_INEXIO is not set # CONFIG_TOUCHSCREEN_MK712 is not set # CONFIG_TOUCHSCREEN_PENMOUNT is not set # CONFIG_TOUCHSCREEN_TOUCHRIGHT is not set # CONFIG_TOUCHSCREEN_TOUCHWIN is not set # CONFIG_TOUCHSCREEN_USB_COMPOSITE is not set # CONFIG_TOUCHSCREEN_TOUCHIT213 is not set # CONFIG_TOUCHSCREEN_TSC2007 is not set # CONFIG_TOUCHSCREEN_W90X900 is not set # CONFIG_TOUCHSCREEN_ST1232 is not set # CONFIG_TOUCHSCREEN_TPS6507X is not set # CONFIG_INPUT_MISC is not set # # Hardware I/O ports # CONFIG_SERIO=y CONFIG_SERIO_SERPORT=y CONFIG_SERIO_LIBPS2=y # CONFIG_SERIO_RAW is not set # CONFIG_SERIO_ALTERA_PS2 is not set # CONFIG_SERIO_PS2MULT is not set # CONFIG_GAMEPORT is not set # # Character devices # CONFIG_VT=y CONFIG_CONSOLE_TRANSLATIONS=y # CONFIG_VT_CONSOLE is not set CONFIG_HW_CONSOLE=y # CONFIG_VT_HW_CONSOLE_BINDING is not set CONFIG_UNIX98_PTYS=y # CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set CONFIG_LEGACY_PTYS=y CONFIG_LEGACY_PTY_COUNT=256 # CONFIG_SERIAL_NONSTANDARD is not set # CONFIG_N_GSM is not set # CONFIG_TRACE_SINK is not set CONFIG_DEVKMEM=y # # Serial drivers # CONFIG_SERIAL_8250=y CONFIG_SERIAL_8250_CONSOLE=y CONFIG_SERIAL_8250_NR_UARTS=3 CONFIG_SERIAL_8250_RUNTIME_UARTS=3 # CONFIG_SERIAL_8250_EXTENDED is not set # # Non-8250 serial port support # CONFIG_SERIAL_CORE=y CONFIG_SERIAL_CORE_CONSOLE=y # CONFIG_SERIAL_TIMBERDALE is not set # CONFIG_SERIAL_ALTERA_JTAGUART is not set # CONFIG_SERIAL_ALTERA_UART is not set # CONFIG_SERIAL_XILINX_PS_UART is not set # CONFIG_TTY_PRINTK is not set # CONFIG_HVC_DCC is not set # CONFIG_IPMI_HANDLER is not set CONFIG_HW_RANDOM=m # CONFIG_HW_RANDOM_TIMERIOMEM is not set # CONFIG_R3964 is not set # CONFIG_RAW_DRIVER is not set # CONFIG_TCG_TPM is not set # CONFIG_RAMOOPS is not set CONFIG_I2C=y CONFIG_I2C_BOARDINFO=y CONFIG_I2C_COMPAT=y CONFIG_I2C_CHARDEV=y # CONFIG_I2C_MUX is not set CONFIG_I2C_HELPER_AUTO=y # # I2C Hardware Bus support # # # I2C system bus drivers (mostly embedded / system-on-chip) # CONFIG_I2C_DAVINCI=y # CONFIG_I2C_DESIGNWARE is not set # CONFIG_I2C_GPIO is not set # CONFIG_I2C_OCORES is not set # CONFIG_I2C_PCA_PLATFORM is not set # CONFIG_I2C_PXA_PCI is not set # CONFIG_I2C_SIMTEC is not set # CONFIG_I2C_XILINX is not set # # External I2C/SMBus adapter drivers # # CONFIG_I2C_DIOLAN_U2C is not set # CONFIG_I2C_PARPORT_LIGHT is not set # CONFIG_I2C_TAOS_EVM is not set # CONFIG_I2C_TINY_USB is not set # # Other I2C/SMBus bus drivers # # CONFIG_I2C_STUB is not set # CONFIG_I2C_DEBUG_CORE is not set # CONFIG_I2C_DEBUG_ALGO is not set # CONFIG_I2C_DEBUG_BUS is not set # CONFIG_SPI is not set # # PPS support # # CONFIG_PPS is not set # # PPS generators support # # # PTP clock support # # # Enable Device Drivers -> PPS to see the PTP clock options. # CONFIG_ARCH_REQUIRE_GPIOLIB=y CONFIG_GPIOLIB=y # CONFIG_DEBUG_GPIO is not set # CONFIG_GPIO_SYSFS is not set # # Memory mapped GPIO drivers: # # CONFIG_GPIO_GENERIC_PLATFORM is not set # CONFIG_GPIO_IT8761E is not set # # I2C GPIO expanders: # # CONFIG_GPIO_MAX7300 is not set # CONFIG_GPIO_MAX732X is not set # CONFIG_GPIO_PCA953X_IRQ is not set CONFIG_GPIO_PCF857X=y # CONFIG_GPIO_SX150X is not set # CONFIG_GPIO_ADP5588 is not set # # PCI GPIO expanders: # # # SPI GPIO expanders: # # CONFIG_GPIO_MCP23S08 is not set # # AC97 GPIO expanders: # # # MODULbus GPIO expanders: # # CONFIG_W1 is not set # CONFIG_POWER_SUPPLY is not set # CONFIG_HWMON is not set # CONFIG_THERMAL is not set CONFIG_WATCHDOG=y # CONFIG_WATCHDOG_CORE is not set # CONFIG_WATCHDOG_NOWAYOUT is not set # # Watchdog Device Drivers # # CONFIG_SOFT_WATCHDOG is not set # CONFIG_DW_WATCHDOG is not set # CONFIG_DAVINCI_WATCHDOG is not set # CONFIG_MAX63XX_WATCHDOG is not set # # USB-based Watchdog Cards # # CONFIG_USBPCWATCHDOG is not set CONFIG_SSB_POSSIBLE=y # # Sonics Silicon Backplane # # CONFIG_SSB is not set CONFIG_BCMA_POSSIBLE=y # # Broadcom specific AMBA # # CONFIG_BCMA is not set CONFIG_MFD_SUPPORT=y # CONFIG_MFD_CORE is not set # CONFIG_MFD_88PM860X is not set # CONFIG_MFD_SM501 is not set # CONFIG_MFD_ASIC3 is not set # CONFIG_HTC_EGPIO is not set # CONFIG_HTC_PASIC3 is not set # CONFIG_HTC_I2CPLD is not set # CONFIG_TPS6105X is not set # CONFIG_TPS65010 is not set # CONFIG_TPS6507X is not set # CONFIG_MFD_TPS6586X is not set # CONFIG_MFD_TPS65910 is not set # CONFIG_MFD_TPS65912_I2C is not set # CONFIG_TWL4030_CORE is not set # CONFIG_MFD_STMPE is not set # CONFIG_MFD_TC3589X is not set # CONFIG_MFD_TMIO is not set # CONFIG_MFD_T7L66XB is not set # CONFIG_MFD_TC6387XB is not set # CONFIG_MFD_TC6393XB is not set # CONFIG_PMIC_DA903X is not set # CONFIG_PMIC_ADP5520 is not set # CONFIG_MFD_MAX8925 is not set # CONFIG_MFD_MAX8997 is not set # CONFIG_MFD_MAX8998 is not set # CONFIG_MFD_WM8400 is not set # CONFIG_MFD_WM831X_I2C is not set # CONFIG_MFD_WM8350_I2C is not set # CONFIG_MFD_WM8994 is not set # CONFIG_MFD_PCF50633 is not set # CONFIG_ABX500_CORE is not set # CONFIG_MFD_WL1273_CORE is not set # CONFIG_MFD_AAT2870_CORE is not set # CONFIG_REGULATOR is not set # CONFIG_MEDIA_SUPPORT is not set # # Graphics support # # CONFIG_DRM is not set # CONFIG_VGASTATE is not set # CONFIG_VIDEO_OUTPUT_CONTROL is not set CONFIG_FB=y # CONFIG_FIRMWARE_EDID is not set # CONFIG_FB_DDC is not set # CONFIG_FB_BOOT_VESA_SUPPORT is not set CONFIG_FB_CFB_FILLRECT=y CONFIG_FB_CFB_COPYAREA=y CONFIG_FB_CFB_IMAGEBLIT=y # CONFIG_FB_CFB_REV_PIXELS_IN_BYTE is not set # CONFIG_FB_SYS_FILLRECT is not set # CONFIG_FB_SYS_COPYAREA is not set # CONFIG_FB_SYS_IMAGEBLIT is not set # CONFIG_FB_FOREIGN_ENDIAN is not set # CONFIG_FB_SYS_FOPS is not set # CONFIG_FB_WMT_GE_ROPS is not set # CONFIG_FB_SVGALIB is not set # CONFIG_FB_MACMODES is not set # CONFIG_FB_BACKLIGHT is not set # CONFIG_FB_MODE_HELPERS is not set # CONFIG_FB_TILEBLITTING is not set # # Frame buffer hardware drivers # # CONFIG_FB_S1D13XXX is not set # CONFIG_FB_UDL is not set CONFIG_FB_DA8XX=y # CONFIG_FB_VIRTUAL is not set # CONFIG_FB_METRONOME is not set # CONFIG_FB_BROADSHEET is not set # CONFIG_BACKLIGHT_LCD_SUPPORT is not set # # Display device support # # CONFIG_DISPLAY_SUPPORT is not set # # Console display driver support # CONFIG_DUMMY_CONSOLE=y # CONFIG_FRAMEBUFFER_CONSOLE is not set CONFIG_LOGO=y CONFIG_LOGO_LINUX_MONO=y CONFIG_LOGO_LINUX_VGA16=y CONFIG_LOGO_LINUX_CLUT224=y CONFIG_SOUND=y # CONFIG_SOUND_OSS_CORE is not set CONFIG_SND=y CONFIG_SND_TIMER=y CONFIG_SND_PCM=y CONFIG_SND_JACK=y # CONFIG_SND_SEQUENCER is not set # CONFIG_SND_MIXER_OSS is not set # CONFIG_SND_PCM_OSS is not set # CONFIG_SND_HRTIMER is not set # CONFIG_SND_DYNAMIC_MINORS is not set CONFIG_SND_SUPPORT_OLD_API=y CONFIG_SND_VERBOSE_PROCFS=y # CONFIG_SND_VERBOSE_PRINTK is not set # CONFIG_SND_DEBUG is not set # CONFIG_SND_RAWMIDI_SEQ is not set # CONFIG_SND_OPL3_LIB_SEQ is not set # CONFIG_SND_OPL4_LIB_SEQ is not set # CONFIG_SND_SBAWE_SEQ is not set # CONFIG_SND_EMU10K1_SEQ is not set CONFIG_SND_DRIVERS=y # CONFIG_SND_DUMMY is not set # CONFIG_SND_ALOOP is not set # CONFIG_SND_MTPAV is not set # CONFIG_SND_SERIAL_U16550 is not set # CONFIG_SND_MPU401 is not set CONFIG_SND_ARM=y CONFIG_SND_USB=y # CONFIG_SND_USB_AUDIO is not set # CONFIG_SND_USB_UA101 is not set # CONFIG_SND_USB_CAIAQ is not set # CONFIG_SND_USB_6FIRE is not set CONFIG_SND_SOC=y # CONFIG_SND_SOC_CACHE_LZO is not set CONFIG_SND_DAVINCI_SOC=y CONFIG_SND_DAVINCI_SOC_MCASP=y CONFIG_SND_OMAPL138_HAWKBOARD=y CONFIG_SND_SOC_I2C_AND_SPI=y # CONFIG_SND_SOC_ALL_CODECS is not set CONFIG_SND_SOC_TLV320AIC3X=y # CONFIG_SOUND_PRIME is not set # CONFIG_HID_SUPPORT is not set CONFIG_USB_SUPPORT=y CONFIG_USB_ARCH_HAS_HCD=y CONFIG_USB_ARCH_HAS_OHCI=y # CONFIG_USB_ARCH_HAS_EHCI is not set CONFIG_USB=y # CONFIG_USB_DEBUG is not set CONFIG_USB_ANNOUNCE_NEW_DEVICES=y # # Miscellaneous USB options # CONFIG_USB_DEVICEFS=y CONFIG_USB_DEVICE_CLASS=y # CONFIG_USB_DYNAMIC_MINORS is not set # CONFIG_USB_OTG_WHITELIST is not set # CONFIG_USB_OTG_BLACKLIST_HUB is not set # CONFIG_USB_MON is not set # CONFIG_USB_WUSB is not set # CONFIG_USB_WUSB_CBAF is not set # # USB Host Controller Drivers # # CONFIG_USB_C67X00_HCD is not set # CONFIG_USB_OXU210HP_HCD is not set # CONFIG_USB_ISP116X_HCD is not set # CONFIG_USB_ISP1760_HCD is not set # CONFIG_USB_ISP1362_HCD is not set CONFIG_USB_OHCI_HCD=y # CONFIG_USB_OHCI_BIG_ENDIAN_DESC is not set # CONFIG_USB_OHCI_BIG_ENDIAN_MMIO is not set CONFIG_USB_OHCI_LITTLE_ENDIAN=y # CONFIG_USB_SL811_HCD is not set # CONFIG_USB_R8A66597_HCD is not set # CONFIG_USB_HWA_HCD is not set # # USB Device Class drivers # # CONFIG_USB_ACM is not set # CONFIG_USB_PRINTER is not set # CONFIG_USB_WDM is not set # CONFIG_USB_TMC is not set # # NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may # # # also be needed; see USB_STORAGE Help for more info # CONFIG_USB_STORAGE=m CONFIG_USB_STORAGE_DEBUG=y # CONFIG_USB_STORAGE_REALTEK is not set # CONFIG_USB_STORAGE_DATAFAB is not set # CONFIG_USB_STORAGE_FREECOM is not set # CONFIG_USB_STORAGE_ISD200 is not set # CONFIG_USB_STORAGE_USBAT is not set # CONFIG_USB_STORAGE_SDDR09 is not set # CONFIG_USB_STORAGE_SDDR55 is not set # CONFIG_USB_STORAGE_JUMPSHOT is not set # CONFIG_USB_STORAGE_ALAUDA is not set # CONFIG_USB_STORAGE_ONETOUCH is not set # CONFIG_USB_STORAGE_KARMA is not set # CONFIG_USB_STORAGE_CYPRESS_ATACB is not set # CONFIG_USB_STORAGE_ENE_UB6250 is not set # CONFIG_USB_UAS is not set # CONFIG_USB_LIBUSUAL is not set # # USB Imaging devices # # CONFIG_USB_MDC800 is not set # CONFIG_USB_MICROTEK is not set # # USB port drivers # # CONFIG_USB_SERIAL is not set # # USB Miscellaneous drivers # # CONFIG_USB_EMI62 is not set # CONFIG_USB_EMI26 is not set # CONFIG_USB_ADUTUX is not set # CONFIG_USB_SEVSEG is not set # CONFIG_USB_RIO500 is not set # CONFIG_USB_LEGOTOWER is not set # CONFIG_USB_LCD is not set # CONFIG_USB_LED is not set # CONFIG_USB_CYPRESS_CY7C63 is not set # CONFIG_USB_CYTHERM is not set # CONFIG_USB_IDMOUSE is not set # CONFIG_USB_FTDI_ELAN is not set # CONFIG_USB_APPLEDISPLAY is not set # CONFIG_USB_LD is not set # CONFIG_USB_TRANCEVIBRATOR is not set # CONFIG_USB_IOWARRIOR is not set # CONFIG_USB_TEST is not set # CONFIG_USB_ISIGHTFW is not set # CONFIG_USB_YUREX is not set # CONFIG_USB_GADGET is not set # # OTG and related infrastructure # # CONFIG_USB_GPIO_VBUS is not set # CONFIG_USB_ULPI is not set # CONFIG_NOP_USB_XCEIV is not set CONFIG_MMC=y # CONFIG_MMC_DEBUG is not set # CONFIG_MMC_UNSAFE_RESUME is not set # CONFIG_MMC_CLKGATE is not set # # MMC/SD/SDIO Card Drivers # CONFIG_MMC_BLOCK=y CONFIG_MMC_BLOCK_MINORS=8 CONFIG_MMC_BLOCK_BOUNCE=y # CONFIG_SDIO_UART is not set # CONFIG_MMC_TEST is not set # # MMC/SD/SDIO Host Controller Drivers # # CONFIG_MMC_SDHCI is not set # CONFIG_MMC_SDHCI_PXAV3 is not set # CONFIG_MMC_SDHCI_PXAV2 is not set CONFIG_MMC_DAVINCI=y # CONFIG_MMC_DW is not set # CONFIG_MMC_VUB300 is not set # CONFIG_MMC_USHC is not set # CONFIG_MEMSTICK is not set # CONFIG_NEW_LEDS is not set # CONFIG_ACCESSIBILITY is not set CONFIG_RTC_LIB=y CONFIG_RTC_CLASS=y CONFIG_RTC_HCTOSYS=y CONFIG_RTC_HCTOSYS_DEVICE="rtc0" # CONFIG_RTC_DEBUG is not set # # RTC interfaces # CONFIG_RTC_INTF_SYSFS=y CONFIG_RTC_INTF_PROC=y CONFIG_RTC_INTF_DEV=y # CONFIG_RTC_INTF_DEV_UIE_EMUL is not set # CONFIG_RTC_DRV_TEST is not set # # I2C RTC drivers # # CONFIG_RTC_DRV_DS1307 is not set # CONFIG_RTC_DRV_DS1374 is not set # CONFIG_RTC_DRV_DS1672 is not set # CONFIG_RTC_DRV_DS3232 is not set # CONFIG_RTC_DRV_MAX6900 is not set # CONFIG_RTC_DRV_RS5C372 is not set # CONFIG_RTC_DRV_ISL1208 is not set # CONFIG_RTC_DRV_ISL12022 is not set # CONFIG_RTC_DRV_X1205 is not set # CONFIG_RTC_DRV_PCF8563 is not set # CONFIG_RTC_DRV_PCF8583 is not set # CONFIG_RTC_DRV_M41T80 is not set # CONFIG_RTC_DRV_BQ32K is not set # CONFIG_RTC_DRV_S35390A is not set # CONFIG_RTC_DRV_FM3130 is not set # CONFIG_RTC_DRV_RX8581 is not set # CONFIG_RTC_DRV_RX8025 is not set # CONFIG_RTC_DRV_EM3027 is not set # CONFIG_RTC_DRV_RV3029C2 is not set # # SPI RTC drivers # # # Platform RTC drivers # # CONFIG_RTC_DRV_CMOS is not set # CONFIG_RTC_DRV_DS1286 is not set # CONFIG_RTC_DRV_DS1511 is not set # CONFIG_RTC_DRV_DS1553 is not set # CONFIG_RTC_DRV_DS1742 is not set # CONFIG_RTC_DRV_STK17TA8 is not set # CONFIG_RTC_DRV_M48T86 is not set # CONFIG_RTC_DRV_M48T35 is not set # CONFIG_RTC_DRV_M48T59 is not set # CONFIG_RTC_DRV_MSM6242 is not set # CONFIG_RTC_DRV_BQ4802 is not set # CONFIG_RTC_DRV_RP5C01 is not set # CONFIG_RTC_DRV_V3020 is not set # # on-CPU RTC drivers # CONFIG_RTC_DRV_OMAP=y # CONFIG_DMADEVICES is not set # CONFIG_AUXDISPLAY is not set # CONFIG_UIO is not set # # Virtio drivers # # CONFIG_VIRTIO_BALLOON is not set # CONFIG_STAGING is not set CONFIG_CLKDEV_LOOKUP=y CONFIG_IOMMU_SUPPORT=y # CONFIG_VIRT_DRIVERS is not set # # File systems # CONFIG_EXT2_FS=y # CONFIG_EXT2_FS_XATTR is not set # CONFIG_EXT2_FS_XIP is not set CONFIG_EXT3_FS=y CONFIG_EXT3_DEFAULTS_TO_ORDERED=y CONFIG_EXT3_FS_XATTR=y # CONFIG_EXT3_FS_POSIX_ACL is not set # CONFIG_EXT3_FS_SECURITY is not set # CONFIG_EXT4_FS is not set CONFIG_JBD=y CONFIG_FS_MBCACHE=y # CONFIG_REISERFS_FS is not set # CONFIG_JFS_FS is not set CONFIG_XFS_FS=m # CONFIG_XFS_QUOTA is not set # CONFIG_XFS_POSIX_ACL is not set # CONFIG_XFS_RT is not set # CONFIG_XFS_DEBUG is not set # CONFIG_GFS2_FS is not set # CONFIG_BTRFS_FS is not set # CONFIG_NILFS2_FS is not set # CONFIG_FS_POSIX_ACL is not set CONFIG_EXPORTFS=m CONFIG_FILE_LOCKING=y CONFIG_FSNOTIFY=y CONFIG_DNOTIFY=y CONFIG_INOTIFY_USER=y # CONFIG_FANOTIFY is not set # CONFIG_QUOTA is not set # CONFIG_QUOTACTL is not set CONFIG_AUTOFS4_FS=m # CONFIG_FUSE_FS is not set # # Caches # # CONFIG_FSCACHE is not set # # CD-ROM/DVD Filesystems # # CONFIG_ISO9660_FS is not set # CONFIG_UDF_FS is not set # # DOS/FAT/NT Filesystems # CONFIG_FAT_FS=y CONFIG_MSDOS_FS=y CONFIG_VFAT_FS=y CONFIG_FAT_DEFAULT_CODEPAGE=437 CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1" # CONFIG_NTFS_FS is not set # # Pseudo filesystems # CONFIG_PROC_FS=y CONFIG_PROC_SYSCTL=y CONFIG_PROC_PAGE_MONITOR=y CONFIG_SYSFS=y CONFIG_TMPFS=y # CONFIG_TMPFS_POSIX_ACL is not set # CONFIG_TMPFS_XATTR is not set # CONFIG_HUGETLB_PAGE is not set # CONFIG_CONFIGFS_FS is not set CONFIG_MISC_FILESYSTEMS=y # CONFIG_ADFS_FS is not set # CONFIG_AFFS_FS is not set # CONFIG_HFS_FS is not set # CONFIG_HFSPLUS_FS is not set # CONFIG_BEFS_FS is not set # CONFIG_BFS_FS is not set # CONFIG_EFS_FS is not set # CONFIG_LOGFS is not set CONFIG_CRAMFS=y # CONFIG_SQUASHFS is not set # CONFIG_VXFS_FS is not set CONFIG_MINIX_FS=m # CONFIG_OMFS_FS is not set # CONFIG_HPFS_FS is not set # CONFIG_QNX4FS_FS is not set # CONFIG_ROMFS_FS is not set # CONFIG_PSTORE is not set # CONFIG_SYSV_FS is not set # CONFIG_UFS_FS is not set CONFIG_NETWORK_FILESYSTEMS=y CONFIG_NFS_FS=y CONFIG_NFS_V3=y # CONFIG_NFS_V3_ACL is not set # CONFIG_NFS_V4 is not set CONFIG_ROOT_NFS=y CONFIG_NFSD=m CONFIG_NFSD_V3=y # CONFIG_NFSD_V3_ACL is not set # CONFIG_NFSD_V4 is not set CONFIG_LOCKD=y CONFIG_LOCKD_V4=y CONFIG_NFS_COMMON=y CONFIG_SUNRPC=y # CONFIG_CEPH_FS is not set # CONFIG_CIFS is not set # CONFIG_NCP_FS is not set # CONFIG_CODA_FS is not set # CONFIG_AFS_FS is not set # # Partition Types # CONFIG_PARTITION_ADVANCED=y # CONFIG_ACORN_PARTITION is not set # CONFIG_OSF_PARTITION is not set # CONFIG_AMIGA_PARTITION is not set # CONFIG_ATARI_PARTITION is not set # CONFIG_MAC_PARTITION is not set CONFIG_MSDOS_PARTITION=y # CONFIG_BSD_DISKLABEL is not set # CONFIG_MINIX_SUBPARTITION is not set # CONFIG_SOLARIS_X86_PARTITION is not set # CONFIG_UNIXWARE_DISKLABEL is not set # CONFIG_LDM_PARTITION is not set # CONFIG_SGI_PARTITION is not set # CONFIG_ULTRIX_PARTITION is not set # CONFIG_SUN_PARTITION is not set # CONFIG_KARMA_PARTITION is not set # CONFIG_EFI_PARTITION is not set # CONFIG_SYSV68_PARTITION is not set CONFIG_NLS=y CONFIG_NLS_DEFAULT="iso8859-1" CONFIG_NLS_CODEPAGE_437=y # CONFIG_NLS_CODEPAGE_737 is not set # CONFIG_NLS_CODEPAGE_775 is not set # CONFIG_NLS_CODEPAGE_850 is not set # CONFIG_NLS_CODEPAGE_852 is not set # CONFIG_NLS_CODEPAGE_855 is not set # CONFIG_NLS_CODEPAGE_857 is not set # CONFIG_NLS_CODEPAGE_860 is not set # CONFIG_NLS_CODEPAGE_861 is not set # CONFIG_NLS_CODEPAGE_862 is not set # CONFIG_NLS_CODEPAGE_863 is not set # CONFIG_NLS_CODEPAGE_864 is not set # CONFIG_NLS_CODEPAGE_865 is not set # CONFIG_NLS_CODEPAGE_866 is not set # CONFIG_NLS_CODEPAGE_869 is not set # CONFIG_NLS_CODEPAGE_936 is not set # CONFIG_NLS_CODEPAGE_950 is not set # CONFIG_NLS_CODEPAGE_932 is not set # CONFIG_NLS_CODEPAGE_949 is not set # CONFIG_NLS_CODEPAGE_874 is not set # CONFIG_NLS_ISO8859_8 is not set # CONFIG_NLS_CODEPAGE_1250 is not set # CONFIG_NLS_CODEPAGE_1251 is not set CONFIG_NLS_ASCII=m CONFIG_NLS_ISO8859_1=y # CONFIG_NLS_ISO8859_2 is not set # CONFIG_NLS_ISO8859_3 is not set # CONFIG_NLS_ISO8859_4 is not set # CONFIG_NLS_ISO8859_5 is not set # CONFIG_NLS_ISO8859_6 is not set # CONFIG_NLS_ISO8859_7 is not set # CONFIG_NLS_ISO8859_9 is not set # CONFIG_NLS_ISO8859_13 is not set # CONFIG_NLS_ISO8859_14 is not set # CONFIG_NLS_ISO8859_15 is not set # CONFIG_NLS_KOI8_R is not set # CONFIG_NLS_KOI8_U is not set CONFIG_NLS_UTF8=m # # Kernel hacking # # CONFIG_PRINTK_TIME is not set CONFIG_DEFAULT_MESSAGE_LOGLEVEL=4 CONFIG_ENABLE_WARN_DEPRECATED=y CONFIG_ENABLE_MUST_CHECK=y CONFIG_FRAME_WARN=1024 # CONFIG_MAGIC_SYSRQ is not set # CONFIG_STRIP_ASM_SYMS is not set # CONFIG_UNUSED_SYMBOLS is not set # CONFIG_DEBUG_FS is not set # CONFIG_HEADERS_CHECK is not set # CONFIG_DEBUG_SECTION_MISMATCH is not set CONFIG_DEBUG_KERNEL=y # CONFIG_DEBUG_SHIRQ is not set # CONFIG_LOCKUP_DETECTOR is not set # CONFIG_HARDLOCKUP_DETECTOR is not set # CONFIG_DETECT_HUNG_TASK is not set # CONFIG_SCHED_DEBUG is not set # CONFIG_SCHEDSTATS is not set # CONFIG_TIMER_STATS is not set # CONFIG_DEBUG_OBJECTS is not set # CONFIG_SLUB_DEBUG_ON is not set # CONFIG_SLUB_STATS is not set # CONFIG_DEBUG_KMEMLEAK is not set # CONFIG_DEBUG_PREEMPT is not set # CONFIG_DEBUG_RT_MUTEXES is not set # CONFIG_RT_MUTEX_TESTER is not set # CONFIG_DEBUG_SPINLOCK is not set # CONFIG_DEBUG_MUTEXES is not set # CONFIG_DEBUG_LOCK_ALLOC is not set # CONFIG_PROVE_LOCKING is not set # CONFIG_SPARSE_RCU_POINTER is not set # CONFIG_LOCK_STAT is not set # CONFIG_DEBUG_ATOMIC_SLEEP is not set # CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set # CONFIG_DEBUG_STACK_USAGE is not set # CONFIG_DEBUG_KOBJECT is not set # CONFIG_DEBUG_BUGVERBOSE is not set # CONFIG_DEBUG_INFO is not set # CONFIG_DEBUG_VM is not set # CONFIG_DEBUG_WRITECOUNT is not set # CONFIG_DEBUG_MEMORY_INIT is not set # CONFIG_DEBUG_LIST is not set # CONFIG_TEST_LIST_SORT is not set # CONFIG_DEBUG_SG is not set # CONFIG_DEBUG_NOTIFIERS is not set # CONFIG_DEBUG_CREDENTIALS is not set # CONFIG_BOOT_PRINTK_DELAY is not set # CONFIG_RCU_TORTURE_TEST is not set CONFIG_RCU_CPU_STALL_TIMEOUT=60 CONFIG_RCU_CPU_STALL_VERBOSE=y # CONFIG_BACKTRACE_SELF_TEST is not set # CONFIG_DEBUG_BLOCK_EXT_DEVT is not set # CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set # CONFIG_FAULT_INJECTION is not set # CONFIG_LATENCYTOP is not set # CONFIG_SYSCTL_SYSCALL_CHECK is not set # CONFIG_DEBUG_PAGEALLOC is not set CONFIG_HAVE_FUNCTION_TRACER=y CONFIG_HAVE_FUNCTION_GRAPH_TRACER=y CONFIG_HAVE_DYNAMIC_FTRACE=y CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y CONFIG_HAVE_C_RECORDMCOUNT=y CONFIG_TRACING_SUPPORT=y CONFIG_FTRACE=y # CONFIG_FUNCTION_TRACER is not set # CONFIG_IRQSOFF_TRACER is not set # CONFIG_PREEMPT_TRACER is not set # CONFIG_SCHED_TRACER is not set # CONFIG_ENABLE_DEFAULT_TRACERS is not set CONFIG_BRANCH_PROFILE_NONE=y # CONFIG_PROFILE_ANNOTATED_BRANCHES is not set # CONFIG_PROFILE_ALL_BRANCHES is not set # CONFIG_STACK_TRACER is not set # CONFIG_BLK_DEV_IO_TRACE is not set # CONFIG_DMA_API_DEBUG is not set # CONFIG_ATOMIC64_SELFTEST is not set # CONFIG_SAMPLES is not set CONFIG_HAVE_ARCH_KGDB=y # CONFIG_KGDB is not set # CONFIG_TEST_KSTRTOX is not set # CONFIG_STRICT_DEVMEM is not set CONFIG_ARM_UNWIND=y CONFIG_DEBUG_USER=y # CONFIG_DEBUG_LL is not set # CONFIG_OC_ETM is not set # # Security options # # CONFIG_KEYS is not set # CONFIG_SECURITY_DMESG_RESTRICT is not set # CONFIG_SECURITY is not set # CONFIG_SECURITYFS is not set CONFIG_DEFAULT_SECURITY_DAC=y CONFIG_DEFAULT_SECURITY="" CONFIG_CRYPTO=y # # Crypto core or helper # # CONFIG_CRYPTO_MANAGER is not set # CONFIG_CRYPTO_MANAGER2 is not set # CONFIG_CRYPTO_GF128MUL is not set # CONFIG_CRYPTO_NULL is not set # CONFIG_CRYPTO_CRYPTD is not set # CONFIG_CRYPTO_AUTHENC is not set # CONFIG_CRYPTO_TEST is not set # # Authenticated Encryption with Associated Data # # CONFIG_CRYPTO_CCM is not set # CONFIG_CRYPTO_GCM is not set # CONFIG_CRYPTO_SEQIV is not set # # Block modes # # CONFIG_CRYPTO_CBC is not set # CONFIG_CRYPTO_CTR is not set # CONFIG_CRYPTO_CTS is not set # CONFIG_CRYPTO_ECB is not set # CONFIG_CRYPTO_LRW is not set # CONFIG_CRYPTO_PCBC is not set # CONFIG_CRYPTO_XTS is not set # # Hash modes # # CONFIG_CRYPTO_HMAC is not set # CONFIG_CRYPTO_XCBC is not set # CONFIG_CRYPTO_VMAC is not set # # Digest # # CONFIG_CRYPTO_CRC32C is not set # CONFIG_CRYPTO_GHASH is not set # CONFIG_CRYPTO_MD4 is not set # CONFIG_CRYPTO_MD5 is not set # CONFIG_CRYPTO_MICHAEL_MIC is not set # CONFIG_CRYPTO_RMD128 is not set # CONFIG_CRYPTO_RMD160 is not set # CONFIG_CRYPTO_RMD256 is not set # CONFIG_CRYPTO_RMD320 is not set # CONFIG_CRYPTO_SHA1 is not set # CONFIG_CRYPTO_SHA256 is not set # CONFIG_CRYPTO_SHA512 is not set # CONFIG_CRYPTO_TGR192 is not set # CONFIG_CRYPTO_WP512 is not set # # Ciphers # # CONFIG_CRYPTO_AES is not set # CONFIG_CRYPTO_ANUBIS is not set # CONFIG_CRYPTO_ARC4 is not set # CONFIG_CRYPTO_BLOWFISH is not set # CONFIG_CRYPTO_CAMELLIA is not set # CONFIG_CRYPTO_CAST5 is not set # CONFIG_CRYPTO_CAST6 is not set # CONFIG_CRYPTO_DES is not set # CONFIG_CRYPTO_FCRYPT is not set # CONFIG_CRYPTO_KHAZAD is not set # CONFIG_CRYPTO_SALSA20 is not set # CONFIG_CRYPTO_SEED is not set # CONFIG_CRYPTO_SERPENT is not set # CONFIG_CRYPTO_TEA is not set # CONFIG_CRYPTO_TWOFISH is not set # # Compression # # CONFIG_CRYPTO_DEFLATE is not set # CONFIG_CRYPTO_ZLIB is not set # CONFIG_CRYPTO_LZO is not set # # Random Number Generation # # CONFIG_CRYPTO_ANSI_CPRNG is not set # CONFIG_CRYPTO_USER_API_HASH is not set # CONFIG_CRYPTO_USER_API_SKCIPHER is not set # CONFIG_CRYPTO_HW is not set # CONFIG_BINARY_PRINTF is not set # # Library routines # CONFIG_BITREVERSE=y CONFIG_CRC_CCITT=m # CONFIG_CRC16 is not set CONFIG_CRC_T10DIF=m # CONFIG_CRC_ITU_T is not set CONFIG_CRC32=y # CONFIG_CRC7 is not set # CONFIG_LIBCRC32C is not set # CONFIG_CRC8 is not set CONFIG_ZLIB_INFLATE=y # CONFIG_XZ_DEC is not set # CONFIG_XZ_DEC_BCJ is not set CONFIG_DECOMPRESS_GZIP=y CONFIG_GENERIC_ALLOCATOR=y CONFIG_HAS_IOMEM=y CONFIG_HAS_IOPORT=y CONFIG_HAS_DMA=y CONFIG_NLATTR=y CONFIG_GENERIC_ATOMIC64=y # CONFIG_AVERAGE is not set # CONFIG_CORDIC is not set
Thanks
Sangly