This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 IPIPE register set

The Montavista  2.6.18 linux kernel contains a header file (include/asm/arch/dm365_ipipe_hw.h) with the IPIPE register set. There it seems to define several registers which are not documented in the DM365 VPFE User's Guide document (SPRUFG8A). These include for example register offset ranges 0x44-0x1CC and 0x1F0-0x228. According to the code these address ranges contain registers for OTF Defect Pixel Correction, Lens Shading Correction, Noise Filtering and CFA interpolation. Is that just an omission from the documentation?

Thanks in advance for your help.