This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 147
Hi,
TPS5402 is used AM437x Industrial EVM.
But minimum on time of TPS5402 is 200ns, so I think that it isn't suitable to output less than 2.4V by 24V input and switching frequency 500kHz.
I think it's better to change a power tree on EVM.
Please make sure you read the forum guidelines first.