Hello - I'm getting a little confused with the maxium DARAM space in the C5532.
www.ti.com/.../tms320c5532.pdf
Says it has 64KB of ram, 8 x 4K x 16-bit words
So 8 x 4096 = 32K 16-bit words or 0x0000 to 0x8000 of addressable 16-bit space (give or take MMR registers and a vector table etc).
Is this correct? As I can happily store and retrieve 16-bit words in my C5532 DSP up to double this 0xFFFF.
Are TI Bytes in this case 16-bit? Should it be 8 x 8K x 16-bits, like I appear to have?
Thanks for your help.