Hi All,
we are using ti-processor-sdk -3.00.00.04 .we are using tisdk-rootfs.tar.gz .rootfs.tar file is 500MB.
we built with yocto setup build core-image-minimal image.But we got 40MB size.
how to add our own scripts while booting in init script.
In /etc/rcS.d contains only two scripts.But tisdk-rootfs-image contains more than two,what is the difference between tisdk-rootfs and core-image minimal image.
And how to optimize rootfs size and boot time for latest ti-processor sdk.
I want to add my own script at /etc/rcS.d.
we followed below link but we are not getting the output.
can any solved this issue .please give me idea
we mentioned boot logs below please find below logs.
U-Boot SPL 2016.05 (Sep 19 2016 - 13:00:05)
Trying to boot from MMC1
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05 (Sep 19 2016 - 13:00:05 +0530)
Watchdog enabled
I2C: ready
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
2587720 bytes read in 170 ms (14.5 MiB/s)
40041 bytes read in 16 ms (2.4 MiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x277c48 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ef3b000, end 8ef47c68 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.12-g3639bea54a (veera@FSETBLR1LX046) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #64 PREEMPT Mon Sep 19 14:27:17 IST 2016
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM-SK
[ 0.000000] cma: Reserved 24 MiB at 0x8d000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64960
[ 0.000000] Kernel command line: console=ttyO0,115200n8 3 root=PARTUUID=00000000-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 227516K/262144K available (4903K kernel code, 207K rwdata, 1664K rodata, 244K init, 227K bss, 10052K reserved, 24576K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff800000 ( 752 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0672004 (6569 kB)
[ 0.000000] .init : 0xc0673000 - 0xc06b0000 ( 244 kB)
[ 0.000000] .data : 0xc06b0000 - 0xc06e3d98 ( 208 kB)
[ 0.000000] .bss : 0xc06e5000 - 0xc071ddfc ( 228 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000015] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000040] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000052] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000488] clocksource_probe: no matching clocksources found
[ 0.000678] Console: colour dummy device 80x30
[ 0.000706] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000713] This ensures that you still see kernel messages. Please
[ 0.000719] update your kernel commandline.
[ 0.000736] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216)
[ 0.089057] pid_max: default: 32768 minimum: 301
[ 0.089188] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089201] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089914] Initializing cgroup subsys io
[ 0.089947] Initializing cgroup subsys memory
[ 0.089984] Initializing cgroup subsys devices
[ 0.090000] Initializing cgroup subsys freezer
[ 0.090014] Initializing cgroup subsys perf_event
[ 0.090028] Initializing cgroup subsys pids
[ 0.090056] CPU: Testing write buffer coherency: ok
[ 0.090477] Setting up static identity map for 0x80008200 - 0x80008258
[ 0.092631] devtmpfs: initialized
[ 0.104226] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.119371] omap_hwmod: debugss: _wait_target_disable failed
[ 0.174711] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.176959] pinctrl core: initialized pinctrl subsystem
[ 0.178359] NET: Registered protocol family 16
[ 0.180719] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.209056] cpuidle: using governor ladder
[ 0.239042] cpuidle: using governor menu
[ 0.243700] OMAP GPIO hardware version 0.1
[ 0.254934] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.297488] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.300785] SCSI subsystem initialized
[ 0.301139] usbcore: registered new interface driver usbfs
[ 0.301212] usbcore: registered new interface driver hub
[ 0.301335] usbcore: registered new device driver usb
[ 0.301851] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.302027] pps_core: LinuxPPS API ver. 1 registered
[ 0.302036] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.302069] PTP clock support registered
[ 0.302826] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.303876] clocksource: Switched to clocksource timer1
[ 0.314816] NET: Registered protocol family 2
[ 0.315628] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.315666] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.315695] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.315787] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.315807] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.315963] NET: Registered protocol family 1
[ 0.316928] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.318953] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.327295] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.329290] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252)
[ 0.329323] io scheduler noop registered
[ 0.329338] io scheduler deadline registered
[ 0.329499] io scheduler cfq registered (default)
[ 0.330778] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.392086] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.396450] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 0.950291] console [ttyS0] enabled
[ 0.955129] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 159, base_baud = 3000000) is a 8250
[ 0.971635] loop: module loaded
[ 0.975912] libphy: Fixed MDIO Bus: probed
[ 1.043943] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.050085] davinci_mdio 4a101000.mdio: detected phy mask ffffffbe
[ 1.057781] libphy: 4a101000.mdio: probed
[ 1.061826] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8740
[ 1.070402] davinci_mdio 4a101000.mdio: phy[6]: device 4a101000.mdio:06, driver SMSC LAN8740
[ 1.079598] cpsw 4a100000.ethernet: Detected MACID = 68:9e:19:84:3d:f7
[ 1.087281] cpsw 4a100000.ethernet: cpsw: Detected MACID = 68:9e:19:84:3d:f9
[ 1.095219] PPP generic driver version 2.4.2
[ 1.099909] usbcore: registered new interface driver cdc_ether
[ 1.105926] usbcore: registered new interface driver cdc_subset
[ 1.111982] usbcore: registered new interface driver qmi_wwan
[ 1.118222] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.124822] ehci-pci: EHCI PCI platform driver
[ 1.129360] ehci-platform: EHCI generic platform driver
[ 1.134815] ehci-omap: OMAP-EHCI Host Controller driver
[ 1.140169] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.146432] ohci-pci: OHCI PCI platform driver
[ 1.150962] ohci-platform: OHCI generic platform driver
[ 1.156712] usbcore: registered new interface driver cdc_wdm
[ 1.162479] usbcore: registered new interface driver usb-storage
[ 1.168671] usbcore: registered new interface driver usbserial
[ 1.174602] usbcore: registered new interface driver option
[ 1.180240] usbserial: USB Serial support registered for GSM modem (1-port)
[ 1.187270] i2c /dev entries driver
[ 1.191423] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.198381] sdhci: Secure Digital Host Controller Interface driver
[ 1.204609] sdhci: Copyright(c) Pierre Ossman
[ 1.209405] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.214175] omap_hsmmc 48060000.mmc: Got WP GPIO
[ 1.364200] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.373690] usbcore: registered new interface driver usbhid
[ 1.379393] usbhid: USB HID core driver
[ 1.383270] omap_hsmmc 481d8000.mmc: card claims to support voltages below defined range
[ 1.391721] nf_conntrack version 0.5.0 (3938 buckets, 15752 max)
[ 1.398934] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.404478] arp_tables: (C) 2002 David S. Miller
[ 1.409257] NET: Registered protocol family 17
[ 1.413830] Key type dns_resolver registered
[ 1.418337] omap_voltage_late_init: Voltage driver support not added
[ 1.425848] ThumbEE CPU extension supported.
[ 1.430194] Registering SWP/SWPB emulation handler
[ 1.442241] mmc0: queuing unknown CIS tuple 0x91 (3 bytes)
[ 1.448576] mmc0: new high speed SDIO card at address 0001
[ 1.454323] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.484250] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.490440] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.495237] omap_hsmmc 48060000.mmc: Got WP GPIO
[ 1.500260] mmc_card_regulator: supplied by vbat
[ 1.544473] vdd_mpu: supplied by vbat
[ 1.553293] lis3_reg: disabling
[ 1.558537] Waiting for root device PARTUUID=00000000-02...
[ 1.795993] mmc1: new high speed SDHC card at address aaaa
[ 1.802240] mmcblk0: mmc1:aaaa SU04G 3.69 GiB
[ 1.808520] mmcblk0: p1 p2
[ 1.910701] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 1.919215] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 1.933121] devtmpfs: mounted
[ 1.937284] Freeing unused kernel memory: 244K (c0673000 - c06b0000)
[ 1.943688] This architecture does not have kernel memory protection.
[ 2.225687] systemd[1]: System time before build time, advancing clock.
[ 2.277341] random: systemd urandom read with 21 bits of entropy available
[ 2.305473] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 )
[ 2.324694] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.07!
[ 2.355660] systemd[1]: Set hostname to <am335x-evm>.
[ 3.024855] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 3.054388] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 3.074787] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 3.104779] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 3.134580] systemd[1]: Listening on Socket.
[ OK ] Listening on Syslog Socket.
[ 3.164579] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 3.195048] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 3.228855] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.255909] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 3.284391] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 3.304350] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.359585] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 3.384889] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 3.414317] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 3.434711] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 3.469634] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 3.518585] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 3.579833] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 3.630061] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 3.680484] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 3.763599] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 3.839904] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 3.904719] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 3.939466] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 3.976095] systemd[1]: Created slice system-getty.slice.
[ 4.002126] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ OK ] Created slice system-getty.slice.
[ 4.076559] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 4.104503] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 4.134425] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 4.165148] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Setup Virtual Console.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Started Remount Root and Kernel File Systems.
Starting udev Coldplug all Devices...e
n Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 5.938341] systemd-journald[71]: Received request to flush runtime journal from PID 1
[ OK ] Started Flush Journal to Persistent Storage.
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started udev Coldplug all Devices.
[ 7.158865] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ OK ] Found device /dev/ttyS0.
[ 7.666026] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ OK ] Found device /dev/ttyS3.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Network Time Synchronization.
[FAILED] Failed to start Update UTMP about System Boot/Shutdown.
See 'systemctl status systemd-update-utmp.service' for details.
[DEPEND] Dependency failed for Update UTMP about System Runlevel Changes.
[ 11.083297] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 11.181110] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 1
[ 11.242021] hub 1-0:1.0: USB hub found
[ 11.274260] hub 1-0:1.0: 1 port detected
[ 11.552102] cfg80211: World regulatory domain updated:
[ 11.574243] cfg80211: DFS Master region: unset
[ 11.578651] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[ 11.604060] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[ 11.612127] cfg80211: (2457000 KHz - 2482000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[ 11.634181] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)
[ 11.649464] cfg80211: (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[ 11.680129] wl18xx_driver wl18xx.0.auto: Direct firmware load for ti-connectivity/wl1271-nvs.bin failed with error -2
[ 11.699342] cfg80211: (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)
[ 11.709099] usb 1-1: new high-speed USB device number 2 using musb-hdrc
[ 11.719327] am335x -> drivers/net/wireless/ti/wlcore/main.c:wl12xx_set_power_on
[ 11.734289] cfg80211: (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)
[ 11.754123] cfg80211: (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)
[ 11.762191] cfg80211: (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)
[ 11.774074] am335x-> drivers/net/wireless/ti/wlcore/io.h:wl1271_power_on
[ 11.880301] option 1-1:1.0: GSM modem (1-port) converter detected
[ 11.904289] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB0
[ 11.925199] option 1-1:1.1: GSM modem (1-port) converter detected
[ 11.943291] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB1
[ 11.964107] option 1-1:1.2: GSM modem (1-port) converter detected
[ 11.980455] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB2
[ 12.006435] option 1-1:1.3: GSM modem (1-port) converter detected
[ 12.016261] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB3
[ 12.036211] option 1-1:1.4: GSM modem (1-port) converter detected
[ 12.056321] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB4
[ 12.077674] qmi_wwan 1-1:1.5: cdc-wdm0: USB WDM device
[ 12.104988] qmi_wwan 1-1:1.5 wwan0: register 'qmi_wwan' at usb-musb-hdrc.1.auto-1, WWAN/QMI device, e2:e7:7e:91:f5:74
[ 12.126808] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[ 12.140149] am335x -> drivers/net/wireless/ti/wlcore/io.h:wl1271_power_off
[ 12.361031] wlcore: loaded
Starting Synchronize System and HW clocks...
[ OK ] Reached target System Time Synchronized.
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started D-Bus System Message Bus.
Starting Network Service...
[ OK ] Started Kernel Logging Service.
Starting uim-sysfs.service...
[ OK ] Started System Logging Service.
Starting Login Service...
Starting Permit User Sessions...
[ 13.540532] am335x-> drivers/net/wireless/ti/wlcore/main.c:wl12xx_set_power_on
[ OK ] Started Network Service.
[ OK ] Started Permit User Sessions.
[ 13.644063] am335x -> drivers/net/wireless/ti/wlcore/io.h:wl1271_power_on
[ 14.134354] wlcore: PHY firmware version: Rev 8.2.0.0.237
[ 14.255448] random: nonblocking pool is initialized
[ 14.262722] wlcore: firmware booted (Rev 8.9.0.0.70)
[ 14.340714] net eth1: initializing cpsw version 1.12 (0)
[ 14.366337] net eth0: initialized cpsw ale version 1.4
[ 14.395002] net eth1: phy found : id is : 0x7c111
[ 14.468343] net eth0: initializing cpsw version 1.12 (0)
[ 14.499068] net eth0: phy found : id is : 0x7c111
[ OK ] Started Login Service.
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Reached target Network.
Starting Network Name Resolution...
[ OK ] Started Network Name Resolution.
[ OK ] Started uim-sysfs.service.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyS0
Arago 2016.07 am335x-evm ttyS0
am335x-evm login:
CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.7 | VT102 | Offline | ttyUSB1