The question relates to the DC reference design TIDEP0059 (CENELEC Band data concentrator). The reference schematic shows the use of a TMS320F28375 processor and AFE032 for the PLC SOM. We have been using the TMS320F28PLC84 processor and AFE301 on our nodes. Could we not use the same processor - with the appropriate firmware (sysbios_g3_plc_dc_F2806x_AFE031_CRC16_MSB_ROM_image.hex from the G3_DC_SDK_Package_v4706) for the three phase data concentrator instead?
We are planning to use the AM3358 processor for the application processor on the DC - instead of AM3359. Would this be acceptable as far as running the binaries supplied (lower mac on the PLC processor and upper mac on the AM3358) go?
Thanks for your help