Other Parts Discussed in Thread: DIT4192, PCM1681
We have an audio board design that takes I2S and outputs in parallel with a DAC (PCM1681) and DIT4192s. The DIT4192 datasheet shows that from 22.05kHz to 96kHz the best fs setting is 256, however for 192kHz it shows 128fs is required and no other fs is supported. We have to use the chip in hw mode so I want to set it once and forget it, is it possible to set the MCLK to 128fs and output all frequencies? The PCM1681 (the other chip on the design) can support all sampling rates via 128fs.
Any help is appreciated!