This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

AM3359: IBIS model USB pins

Intellectual 410 points

Replies: 6

Views: 1002

Part Number: AM3359

HI,

I am using AM3359 processor.

PIN No. N18(USB0_DM),N17(USB0_DP)  these pins are marked as NC in the IBIS model.

How to change these pins as driver and receiver.

I want configure these as driver and receiver .

Thanks and Regards,

-Arun

  • The factory team have been notified. They will respond here.

     

    Best Regards
    Biser
  • In reply to Biser Gatchev-XID:

    HI Biser,

    Any update from your factory team?

    Thanks and Regards,

    Arun

  • In reply to Arun Kumar39:

    I have escalated the request.

     

    Best Regards
    Biser
  • Hi Arun,

    The USB DM and DP pins are implemented as analog cells in the AM3359. The IBIS model for that device is implemented for IBIS revision 4.1 which does not support the simulation of analog cells. Therefore, we don't support IBIS modeling of the USB interface for that part. 

    Regards,

    Bill

    If you need more help, please reply back. If your question is answered, please click  Verify Answer 

  • In reply to Bill Taboada:

    Hi Bill,

    Thanks for your reply

    Will you share the updated IBIS file which having USB DP and DM?

    I am requesting you to share the IBIS file ASAP.

    Thanks and Regards,

    Arun

  • In reply to Arun Kumar39:

    Hi Arun,

    At this time there are no plans to update the IBIS model for the AM3359. I will check with the design team to see if there is a model for the USB IOs but I do not expect any updates in the near future.

    Regards,

    Bill

    If you need more help, please reply back. If your question is answered, please click  Verify Answer 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.