This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2X: VIP Slice Port A/B capture resolution in multiplexed mode

Other Parts Discussed in Thread: TIDA-00455

Hi!

TIDA-00455 is designed to capture 4 HD streams (through FPDLink and OV490) on two ports of one slice of VIP on TDA.

Each port(PortA/PortB) of a VIP slice is capturing data in multiplexing mode.

According to TDA2x TRM(as I understand it) this scenario is not available.

Table 9-13 in chapter <9.4.5.8.1 Multiplexing Scenarios>  shows:

Maximum Channels in Dual 8-                 Inerface Clock Rate(MHz)
bit Data Interface Mode -
Interleaved Channels per
Single 8-bit Port.
One 16-bit VIP can be
configured to support two such
8-bit ports.

HD Progressive  n/a                                                              148.5

Can somebody explain me, is my understanding wrong or is it a conflict? Is it possible to capture 2 multiplexed HD streams on one 8-bit port in TDA2x?

Thank you.