This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 739
Part Number: DRA710
Hi All!
I found in the DS that the recommended PMIC solutions are the:
For the DRA71x devices:
TPS65919
or
LP8733
And for the DRA72x devices:
TPS659039
TPS65917
Does it mean that one of these devices can completely power up all the rails on the DRA devices?
Also in case we want to use the device in a standby mode, is there a backup LDO pin that we can use? This to avoid the DC/DC to switch for a very light load....
Do you have maybe an example of how does a fairly optimized power tree look like?
Thanks in advance for your help!
Daniel
In reply to Yordan Kamenov:
Hello Daniel,
I think the user's guides will describe the recommended power solutions. You are right that both of the options can support the processor power.
For DRA72x, the user's guide links are below (also found on the product folders).
TPS659039-Q1 user's guide for DRA72x
TPS65917-Q1 user's guide for DRA72x
TPS65917-Q1 is more optimized with smaller size and space, and would generally be the recommended PMIC. However, if you want PCB-compatibility with a DRA74x or DRA75x solution, you would consider TPS659039-Q1 since it can support both DRA72x and DRA74x/75x.
For DRA71x, the user's guide links are below (also found on the product folders).
TPS65917/9-Q1 user's guide for DRA71x
LP873x user's guide for DRA71x
Note that the LP873x solution is an LP8733-Q1 + LP8732-Q1 2-chip solution. This solution will be lower cost, but also can only support up to 3A on the core rails. If you need up to 3.5A, then use TPS65919-Q1. And if you need higher than 3.5A, use the TPS65917-Q1 solution.
Regards,Karl