Part Number: CC1310
1.IO can be easily reused.I would like to ask if I see SSI is the same as spi.
2.External regulator mode, I am the power supply system of 1.8v, and VDDR_RF is also connected with VDDS to 1.8v, which will not affect my RF performance at 1.8V voltage.
3. The bandwidth of RF matching (868MHZ)
4. Is there any reference design for the voltage part of the 1.8v system for CC1310?