I want IBIS MODEL for circuit simulation.
But I can not get it from HP.
Where can I get it?
Please let me know.
Product name:TMS320VC5416ZGU160
Best Regard,
Nori Takahashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want IBIS MODEL for circuit simulation.
But I can not get it from HP.
Where can I get it?
Please let me know.
Product name:TMS320VC5416ZGU160
Best Regard,
Nori Takahashi
Hi Takahashi-san,
See attached the IBIS files for TMS320VC5416 GGU and PGE packages.
/cfs-file/__key/communityserver-discussions-components-files/791/3463.5416_5F00_ggu.ibs
/cfs-file/__key/communityserver-discussions-components-files/791/0702.5416_5F00_pge.ibs
Regards,
Mark
As far as I can tell, the only difference between GGU and ZGU is that ZGU is lead free while GGU is not lead free.
The two packages are otherwise identical. See here:
http://www.ti.com/packaging/docs/searchtipackages.tsp?packageName=BGA
ZGU (S-PBGA-N144) http://www.ti.com/lit/ml/mpbg279a/mpbg279a.pdf
GGU (S–PBGA–N144) http://www.ti.com/lit/ml/mpbg021c/mpbg021c.pdf
I will just confirm that the IBIS model for GGU can be used instead of ZGU without any impact. I do not expect the IBIS model to change due to the lead free package.
Regards,
Mark
Hi,
Just following up to say that I have confirmed that the IBIS model for GGU can indeed be used instead of the IBIS model for ZGU (Pb-Free).
Regards,
Mark