This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TMS320C5534: Some Question in tms320c5534 Crystal input

Prodigy 10 points

Replies: 1

Views: 145

Part Number: TMS320C5534

Anybody know TMS320C5534 can fit 16mhz crystal input? I want to complete with AT86RF233-AU. Thx alot.

  • See Section 5.7.4.3 PLLs, Table 5-10. PLL Clock Frequency Ranges and Section 5.7.4.3.3.2 CLKIN Pin With LVCMOS-Compatible Clock Input (Optional). The recommendation is:
    11.2896 MHz
    12 MHz
    12.288 MHz

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.