Part Number: DDC112
Thanks for your reply.
1.After check:My VREF is very good,and the chip and circuit is the same as the datasheet.
2.My DCKL frequency is 9MHz, it is created by stm32F1 SPI peripheral and 8Xprescaled from 72MHz to 9MHz.
3.My DDC112 range setting is rang1(12.5pF).
4.My data result using TEST mode as below
test condition:(1.two channel and unit is fA; 2.Integrating time is 1000ms; 3.range1;):
ch1:13628.01 ch2:13628.11fA
ch1:13397.00 ch2:13402.51fA
ch1:13628.44 ch2:13629.47fA
ch1:13397.80 ch2:13402.84fA
ch1:13627.92 ch2:13628.95fA
ch1:13396.72 ch2:13403.21fA
ch1:13628.53 ch2:13628.15fA
ch1:13396.58 ch2:13402.18fA
ch1:13627.97 ch2:13629.75fA
ch1:13397.10 ch2:13403.12fA
ch1:13628.58 ch2:13629.90fA
ch1:13397.85 ch2:13402.22fA
ch1:13627.50 ch2:13628.86fA
ch1:13397.00 ch2:13401.33fA
ch1:13627.97 ch2:13629.24fA
ch1:13397.52 ch2:13402.93fA
test condition:(1.two channel and unit is pA; 2.Integrating time is 10ms; 3.range1;):
ch1:1341.40 ch2:1341.93pA
ch1:1364.61 ch2:1364.79pA
ch1:1341.51 ch2:1341.89pA
ch1:1341.47 ch2:1341.97pA
ch1:1364.60 ch2:1364.68pA
ch1:1341.44 ch2:1341.88pA
ch1:1364.60 ch2:1364.67pA
ch1:1341.49 ch2:1341.97pA
ch1:1341.52 ch2:1341.98pA
ch1:1364.53 ch2:1364.69pA
ch1:1364.58 ch2:1364.67pA
ch1:1364.59 ch2:1364.79pA
ch1:1341.46 ch2:1341.97pA
ch1:1341.42 ch2:1341.89pA
ch1:1341.46 ch2:1341.97pA
ch1:1364.54 ch2:1364.80pA
ch1:1364.62 ch2:1364.69pA
ch1:1341.42 ch2:1341.98pA
ch1:1364.65 ch2:1364.80pA
ch1:1341.44 ch2:1341.99pA
ch1:1364.63 ch2:1364.79pA
ch1:1364.58 ch2:1364.68pA
ch1:1341.48 ch2:1342.00pA
ch1:1364.62 ch2:1364.67pA
ch1:1341.39 ch2:1341.97pA
ch1:1364.61 ch2:1364.67pA
ch1:1341.44 ch2:1341.98pA
ch1:1341.38 ch2:1341.99pA
ch1:1364.56 ch2:1364.78pA
ch1:1341.42 ch2:1341.98pA
ch1:1364.58 ch2:1364.71pA
ch1:1341.46 ch2:1341.94pA
ch1:1341.45 ch2:1341.94pA
There is fluction still, why?
Some one tell me it is because 50Hz power noise. But I think that the 1000ms integrating time should average this noise.
Waiting for your help.
Thanks