Hi ,
I migrate to the new version SDK PROCESSOR_SDK_VISION_03_05_00_0,
And in the TIDL OD usecase, I modified it from video-input to camera-input.
And it runs properly but i observe some frame drop after the initial frame.
(Initial is 30 fps but it will drop to 23 after some frames)
I wonder if i have some mistake when i modified the usecase files.
The old version SDK PROCESSOR_SDK_VISION_03_04_00_0 does not have this issue.
Below files are the usecase log and the modified files.
Thank you in advance.
Best Regards,
Eric Lai