Tool/software: TI-RTOS
Hi
I am using evmAM5728 board and I use CCS v8 (windows) and built VIP loopback example and generated .out using RTOS SDK(processor_sdk_rtos_am57xx_5_00_00_15). Now I want to load .out into the board ,so I can run the program after the power is on again.
When I searched for that I found it can done using boot process using SBL
Step 1. to create Bootable SDCard
2.Copy app and MLO files into SDCard
3.Insert the SDCard into EVM and power on.
Can I copy the app file generated under vip ccs project Debug path into SD Card at the boot up, will it work?
Please correct me if I am wrong.
Thanks,
Jahnavi