Hi,
We are using 66AK2E05XABDA25 in our design. Please provide MTBF/FIT data so that we can proceed with the reliability analysis.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are using 66AK2E05XABDA25 in our design. Please provide MTBF/FIT data so that we can proceed with the reliability analysis.
Thanks
Ameen,
Accurate MTBF / FIT / DPPM measurements require large data sets over years of measurement. We have not accumulated enough historical data for this device to provide high confidence numbers yet. Once we do, the tables on the product page at the following link will be populated:
Until that information is available, the following is the only answer available: 66AK2Exx devices are manufactured on the 28nm HP wafer process node, with goal of ≤ 50 FIT through 100k device POH, when used under datasheet conditions at 105 C junction temperature. The device is fully qualified and tests indicate that it should meet that target.
Tom