hello, i use slh_OMAP-L138.exe
i do
slh_omap-l138 -p COM1 -waitForDevice "c:\boot\u-boot.ais"
from command prompt im getting the following:
Entering AIS Parser
Waiting for the OMAP-L138...
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 15236-Byte section to address 0x80000000.
.........
however i wish to save the output above, for example save all those output into a text file, i tried the following command but it crash
slh_omap-l138 -p COM1 -waitForDevice "c:\boot\u-boot.ais" >c:\boot\log.txt
do anyone know how to log the output into a file?
thank you