Team,
- What is the ESD rating via the human body model? ESD information is not provided in the datasheet.
- If it is possible, what is the peak power or peak energy that any I/O pin can withstand during a transient event (i.e. lightning @ 1000us).
- The absolute maximum rating for any I/O pin is -0.3V to 0.5V assuming no power. Is this rating only applies during steady state condition? What about during transient events?
- What is the overall ON and OFF resistances on each I/O pins?
- From the application note (SPRAA87A), on section 4.1-Design Checklist, it appears that the EMU signals can work as unidirectional with a slow baud rate due to only one mode (Emulation/Normal Mode). However, the datasheet specified the opposite for this emulation signals. Are these emulation signals bidirectional with high baud rate (MHz range)?
Thank you.