This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jitendra,
jitendra yadav said:1. GS2970 ic compatable to drive 16 bit ycbcr format?
are from your side is there any ic which takes sdi serial input and provide 16 bit ycbcr output?
I can not advice regarding GS2970 device or other SDI Deserializer. I can advice only from DM816x device side. For questions related to SDI Deserializers, you can ask post in below e2e forum:
You can also check if below e2e threads will be in help:
jitendra yadav said:2. GS2972 ic compatable to receive 20-bit G/Y/YC format?
are from your side is there any ic which takes 20-bit G/Y/YC data and convert to HD-SDI output?
I can not advice regarding GS2970 device or other SDI Deserializer. I can advice only from DM816x device side.
jitendra yadav said:3.Please provide the reference schematics to implement HD-SDI input and output interfacing with TMS320DM8168?
I do not have such reference design. You can check the DM816x available reference designs at below link:
Regards,
Pavel