Hi,
When using simultaneously the 2 UPP channels in the OMAP L 138 in transmission, are both channels synchronous (Transmit on both channels at the same time) ?
what is the minimum size (in term of byte) for a line? what is the minimum size (in term of line) for a window?
Is OMAP L138 able to manage several windows of different sizes? or same size?
Does the DMA controller allow to jump to another window when the transmission of the 1st window is complete?
Can we manage a sequence or a loop with few windows in the case of transmission?