Other Parts Discussed in Thread: ALP, USB2ANY
Team,
My customer is asking how do you debug TDA2PX Fusion board with ALP tool and USB2ANY debugger?
Is there a minimum length that is required for FPD-Lin cable?
What value should register 0xD5 (AEQ MIN-MAX value) in UB960 Deserializer be set to?
Any other registers need to be modified if they are using a 0.5 feet FPD Cable?
Here is the issue, and things they have tried so far:
I have a USB2ANY debugging device, which is used with ALP GUI tool for debugging register values and Margin analysis. The problem is that USB2ANY Explorer.exe (C:\Program Files (x86)\Texas Instruments\USB2ANY Explorer\Bin) application asks me to update the firmware in it to v2.8 but when I open ALP tool, it asks me to reset it 2.7. If I don't upgrade it back to 2.7, then ALP doesn't open. I am testing my fusion board-TDA2PxEVM for finding out the FPD-Link locking conditions when I use shorter FPD coax cables (length: 0.5 feet). The hardware is working perfectly when I try with 16ft FPD-Link cable. I tried uploading the new firmware (v2.7) provided by Vishy in another e2e link as well but it doesn't solve the issue and I am getting UNKNOWN FPD-Link Deserializer in the Device Information tab.
We appreciate your help!
Thanks
Viktorija