Other Parts Discussed in Thread: TMDSEMU200-U
Hello,
we plan to use the emulator TMDSEMU200-U with TMS320C6654 and there is overwhelming amount of information in the forums. I would like to use the 14 position header to connect the emulator and it uses EMU0 and EMU1. The emulator also comes with a 20 position header which uses in addition EMU2, EMU3 and EMU4. Are they used and is there a loss in function if we use the 14 versus the 20 position headers? We are familiar with the 14 and have used with other TI DSPs and also have the parts in stock.
Is it okay to use the 14 position header with TMDSEMU200-U
I have gone through spru655i and spru641 but I wasn't clear.
Thanks,
Divakar