After making the pinmux changes in the .dts file, how to recompile the kernel and the device tree source using the following commands.
step1 : Add the PATH environment variable.
step2 : kernel sources are clean.
step3 : i have changed led name and pin mux in file of am335x-evmsk.dts.
These steps are completed.
step4 : Then device tree is not compiled. As show in below figure.