HI,
In one of my project I am using Sitara AM5728 processor, ARM is on Linux and DSP is on RTOS. I am seeing the below error when I try to unbind the DSP.
[ 2358.831042] remoteproc remoteproc2: failed to unmap 94371840/100663296
[ 2358.832915] remoteproc remoteproc2: failed to unmap 100663296/0
[ 2358.852049] remoteproc remoteproc2: crash detected in 40800000.dsp: type mmufault
[ 2358.859577] omap-iommu 40d02000.mmu: 40d02000.mmu: errs:0x00000002 da:0x95163980 pgd:0xeb7ee544 *pgd:px00000000
Address "0x95163980" is in range of data section defined in the"Resource table" and ".bld" file. I checked ".map" file but I could not trace where particularly this memory is being used.
Attached is the ".map"file. How to resolve this issue?
Thanks,
Janardan