This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TDA3MV: Question about TDA3 VIN MIPI function

Intellectual 320 points

Replies: 4

Views: 96

Part Number: TDA3MV

Hi TI,

For the TDA3 VIN  MIPI port, does it can separate the data per input port(each DS90UB936 RIN port connect different camera sensor) deserialized from DS90UB936?

BR

jason_koo

  • Hi Jason,

    I am sorry i could not get the question. 

    Once cameras are connected to Desrializer, Deserializer merges/multiplexes them and send them over a single CSI interface. They dont have to be connected to different CSI input ports..

    Rgds,

    Brijesh

  • In reply to Brijesh Jadav:

  • In reply to user5775211:

    Hi Brijesh,

    attached is the function we want to realize, is it workable by this architecture?

    BRs

    Jason Koo

  • In reply to user5775211:

    Hi Jason,

    Yes, it is possible from the capture point of view.

    But there is only one display output for HD resolution, the other display output is TV output. 

    So either you could merge both the camera output into one and then display or display each camera input one by one.

    Rgds,

    Brijesh

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.