Hi,
Can I use a GPIO1_xx pin to wake up the processor from standby mode or is this functionality limited to the GPIO0_xx port?
I'm confused because looking at the register description (Section 25.4.1 in the TRM) I have the impression that there are "GPIO_IRQWAKEN_0" for all GPIOs but in the "Low Power Design Guide" (SPRAC74A–February 2017 / Section 2.2.3) only GPIO0 is listed as possible wake up source.
Thank you for your help!
Reto