Hi Mayank,
Many thanks for your reply.
It is valued to understand the sensor register. I updated the few things as per your reference and modified the setting base on datasheet.
Currently i2c read and write operation is happening, but after few operation its' giving the "GIO_submit:retVal = 0xffffffeb " error
Here is the log snippet.
----------------------------------------------------------------------------
[IPU1-0] 30.168730 s:
[IPU1-0] 30.169005 s: i2cMdSubmitChan: i2c4 transfer to slave address 0x36 failed
[IPU1-0] 30.169157 s: GIO_submit:retVal = 0xffffffeb
[IPU1-0] 30.169218 s: src/bsp_deviceI2c.c @ Line 351:
[IPU1-0] 30.169310 s: I2C4: DEV 0x36: RD 0x19 ... ERROR !!!
[IPU1-0] 30.169401 s: src/bsp_deviceI2c.c @ Line 418:
[IPU1-0] 30.169493 s: I2C4: Error timeout 1 ms!!!
[IPU1-0] 30.169584 s: BspOsal_semPost enabled
[IPU1-0] 30.169645 s: GIO_submit3:retVal = 0xffffffeb
-----------------------------------------------------------------------------------
Pls help to check.
Thanks
Mausam Sinha