This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-OMAPL138: There was missing information about the sample build of the SDK.

Part Number: PROCESSOR-SDK-OMAPL138
Other Parts Discussed in Thread: OMAPL138, CCSTUDIO, MATHLIB

I installed ti-processor-sdk-rtos-omapl138-lcdk-06.00.07-Windows-x86-Install.exe, but i don't create a sample SDK.

CCS9.1 (CCS9.1.0.00010_win64.zip) is installed in C:TI.

Processor-SDK-ti-processor-sdk-rtos-omapl138-lcdk-06.00.00.07-Windows-x86-Install.exe_ is installed in the default folder.

run setupenv.bat at c:tiprocessor_sdk_rtos_omapl138_6_00_00_07.

run benchmarkProjectCreate.bat at c:tiprocessor_sdk_rtos_omapl138_6_00_00_07demosaudio-benchmark-starterkit.

Check environment variables with the set command.

c:\ti\processor_sdk_rtos_omapl138_6_00_00_07\demos\audio-benchmark-starterkit>set
ALLUSERSPROFILE=C:\ProgramData
APPDATA=C:\Users\terui\AppData\Roaming
AUTO_CREATE_COMMAND=eclipse\eclipsec -noSplash
BOARD_ARG=OMAPL138
CCS_DEVICE="com.ti.ccstudio.deviceModel.C6000.GenericC674xDevice"
CCS_INSTALL_PATH=C:/ti/ccsv8
CommonProgramFiles=C:\Program Files\Common Files
CommonProgramFiles(x86)=C:\Program Files (x86)\Common Files
CommonProgramW6432=C:\Program Files\Common Files
COMPUTERNAME=TERUI-PC
ComSpec=C:\WINDOWS\system32\cmd.exe
configsetroot=C:\WINDOWS\ConfigSetRoot
CORE=c674
DriverData=C:\Windows\System32\Drivers\DriverData
DSPLIB_INSTALL_PATH =C:/ti/dsplib_c674x_3_4_0_3
DSPLIB_VERSION=3_4_0_3
ENDIAN=little
endian_list=little
FP_NO_HOST_CHECK=NO
GMAKE_INSTALL_PATH=C:/ti/xdctools_3_51_01_18_core
HOMEDRIVE=C:
HOMEPATH=\Users\terui
IPC_PLATFORM=OMAPL138
IS_CCS_VERSION_4=no
IS_SIMULATOR_SUPPORT_NEEDED=no
LOCALAPPDATA=C:\Users\terui\AppData\Local
LOGONSERVER=\\TERUI-PC
MACROS_FILE=c:\ti\PROCES~1\demos\AUDIO-~1\\macros.ini
MATHLIB_INSTALL_PATH =C:/ti/mathlib_c674x_3_1_2_3
MATHLIB_VERSION=3_1_2_3
MODULE_ARG=""
module_list= all FFT FIR IIR
MY_WORKSPACE=c:\ti\PROCES~1\demos\AUDIO-~1\\BenchmarkProjects
NUMBER_OF_PROCESSORS=8
OneDrive=C:\Users\terui\OneDrive
OS=Windows_NT
OUTPUT_FORMAT=ELF
Path=C:\ti\xdctools_3_51_01_18_core;C:\Program Files (x86)\Common Files\Oracle\Java\javapath;C:\ProgramData\Oracle\Java\javapath;C:\Program Files\ImageMagick-6.8.9-Q16;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files\TortoiseSVN\bin;C:\Program Files (x86)\Microsoft SQL Server\100\Tools\Binn\;C:\Program Files\Microsoft SQL Server\100\Tools\Binn\;C:\Program Files\Microsoft SQL Server\100\DTS\Binn\;C:\Program Files (x86)\SciTools/bin/pc-win32;C:\Program Files (x86)\WinMerge;C:\Program Files (x86)\Skype\Phone\;C:\Program Files (x86)\Microchip\xc16\v1.26\bin;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WINDOWS\System32\WindowsPowerShell\v1.0\;C:\Program Files\dotnet\;C:\Program Files\Microsoft SQL Server\130\Tools\Binn\;C:\WINDOWS\System32\OpenSSH\;C:\Program Files\Microsoft VS Code\bin;C:\Users\terui\Anaconda3;C:\Users\terui\Anaconda3\Library\bin;C:\Users\terui\Anaconda3\Scripts;C:\Users\terui\AppData\Local\Microsoft\WindowsApps;C:\Program Files\JetBrains\PyCharm Community Edition 2018.3.3\bin
PATHEXT=.COM;.EXE;.BAT;.CMD;.VBS;.VBE;.JS;.JSE;.WSF;.WSH;.MSC
PDK_INSTALL_PATH =C:/ti/pdk_omapl138_1_0_9
PDK_PARTNO=OMAPL138
PDK_SHORT_NAME=c:\ti\PROCES~1\demos\AUDIO-~1\
PDK_SOC=omapl138
PDK_VERSION=1_0_9
PROCESSOR=dsp
PROCESSOR_ARCHITECTURE=AMD64
PROCESSOR_IDENTIFIER=Intel64 Family 6 Model 30 Stepping 5, GenuineIntel
PROCESSOR_LEVEL=6
PROCESSOR_REVISION=1e05
proc_list=dsp
PROC_SDK_INSTALL_PATH=C:/ti/processor_sdk_rtos_omapl138_6_00_00_07
PROC_SDK_VERSION=omapl138_6_00_00_07
ProgramData=C:\ProgramData
ProgramFiles=C:\Program Files
ProgramFiles(x86)=C:\Program Files (x86)
ProgramW6432=C:\Program Files
project_detected = 1
PROMPT=$P$G
PSModulePath=C:\WINDOWS\system32\WindowsPowerShell\v1.0\Modules\
PUBLIC=C:\Users\Public
PyCharm Community Edition=C:\Program Files\JetBrains\PyCharm Community Edition 2018.3.3\bin;
RTSC_PLATFORM_NAME=ti.platforms.evm6748
RTSC_TARGET=ti.targets.elf.C674
RULES_MAKE=C:/ti/pdk_omapl138_1_0_9/packages/Rules.make
SDK_INSTALL_PATH=C:/ti
SOC=omapl138
SOC_ARG=OMAPL138
soc_list=K2G K2H K2E C667x C665x AM571x AM572x AM574x OMAPL138 OMAPL137 C6747 C6748
SystemDrive=C:
SystemRoot=C:\WINDOWS
TEMP=C:\Users\terui\AppData\Local\Temp
tempVar1=OMAPL138
TMP=C:\Users\terui\AppData\Local\Temp
TOOLS_INSTALL_PATH=C:/ti
USERDOMAIN=terui-PC
USERDOMAIN_ROAMINGPROFILE=terui-PC
USERNAME=terui
USERPROFILE=C:\Users\terui
VS100COMNTOOLS=C:\Program Files (x86)\Microsoft Visual Studio 10.0\Common7\Tools\
windir=C:\WINDOWS
XDC_VERSION=3_51_01_18_core

It's done so far, but it's not created. What is the cause?