I just received my TMDSSK3358 and I'm able to set the IP and netmask for each interface using ifconfig, and demonstrate the dual MAC mode works. Is there an easy way to put the dev board in switch mode from the command line? Or, do I have to change kernel options and device tree to put into switch mode? I'm looking for a way to switch between dual MAC mode and switch mode "on the fly", or at lease have the mode selected at boot based on an I/O line. Is this possible?
Regards,
Daven