Hi,
I am working on making the Nucleus image to load and run from SD card, for this I am using the TI SBL boot-loader available under processor_sdk_rtos.
To create the app file from the Nucleus.out file, I am using the AM57xImageGen.bat script file located under scripts folder. Once app file is generated I am copying the app and MLO files to bootable SD card. The SBL is running good but it's stuck at Jumping to user application.
What are the change required in Nucleus RTOS application? Apart from the memory mapping any other modifications required? in memory mapping what are the sections should I include, just changing the RAM location from 0x80000000 to 0x80000400 will be sufficient?
I have tested the Nucleus image which I am using with Lauterbach Trace 32 debugger and it's working, the debugger usually initialize the board with CMM script files(.gel files in case of CCS) and loads and runs the application.
Regards,
Naveen.