Other Parts Discussed in Thread: TMDSIDK574
$ sudo apt-get install git build-essential python diffstat texinfo gawk chrpath dos2unix wget unzip socat doxygen libc6:i386 libncurses5:i386 libstdc++6:i386 libz1:i386
$ sudo dpkg-reconfigure dash
Select "No" when prompted.
$ wget releases.linaro.org/.../gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf.tar.xz
$ tar -Jxvf gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf.tar.xz -C $HOME
$ git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk
$ cd tisdk
$ ./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-04.01.00.06-x11-config.txt
$ cd build
$ . conf/setenv
$ export PATH=$HOME/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:$PATH
$ MACHINE=am57xx-evm ARAGO_RT_ENABLE=1 bitbake tisdk-rootfs-image
am57x@am57x:~/tisdk/build$ . conf/setenv
am57x@am57x:~/tisdk/build$ MACHINE=am57xx-evm ARAGO_RT_ENABLE=1 bitbake tisdk-rootfs-image
Loading cache: 100% |##################################################################################################################################################| Time: 0:00:01
Loaded 3259 entries from dependency cache.
WARNING: No recipes available for:
/home/am57x/tisdk/sources/meta-openamp/recipes-bsp/device-tree/device-tree-generation_%.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.32.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am57xx-evm"
DISTRO = "arago"
DISTRO_VERSION = "2017.06"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:cb3ee0c165ef4e71e1aad16812652ca1371a9c80"
meta-arago-distro
meta-arago-extras = "HEAD:8f49ed67d0627a04ac72fd388fda7756273ba2d7"
meta-browser = "HEAD:08576b03af624b65ad949c410d84c11c7d1f2e39"
meta-openamp = "HEAD:8a214032bfb7e8124bc1485c70c69f7d60abb819"
meta-qt5 = "HEAD:2c9f0e4eb0e9097f6f872ec1e1d81768a8ab5f1b"
meta-networking
meta-ruby
meta-python
meta-oe
meta-gnome = "HEAD:fe5c83312de11e80b85680ef237f8acb04b4b26e"
meta-ti = "HEAD:a18d57af8384ced25996739bb66d197c69efb77b"
meta-linaro-toolchain
meta-optee = "HEAD:49b0f32d7e955f250b0022d1b2f403f45a2c2d9c"
meta = "HEAD:e3911133ee9aad7cc3ae89faea80a097f6614fab"
Initialising tasks: 100% |#############################################################################################################################################| Time: 0:00:17
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: mobile-broadband-provider-info-1_20151214-r0 do_fetch: Failed to fetch URL git://git.gnome.org/mobile-broadband-provider-info, attempting MIRRORS if available
WARNING: ofono-1.18-r0 do_fetch: Failed to fetch URL kernel.org/.../ofono-1.18.tar.xz, attempting MIRRORS if available
WARNING: binutils-native-linaro-2.27-r2016.10 do_fetch: Failed to fetch URL git://git.linaro.org/toolchain/binutils-gdb.git;protocol=https;branch=linaro_binutils-2_27-branch, attempting MIRRORS if available
ERROR: binutils-native-linaro-2.27-r2016.10 do_fetch: Fetcher failure: Fetch command export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-RqzreQgfju"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export no_proxy="localhost,127.0.0.0/8,::1"; export NO_PROXY="localhost,127.0.0.0/8,::1"; export https_proxy="http://127.0.0.1:38755/"; export HTTPS_PROXY="http://127.0.0.1:38755/"; export http_proxy="http://127.0.0.1:38755/"; export HTTP_PROXY="http://127.0.0.1:38755/"; export PATH="/home/am57x/tisdk/sources/oe-core/scripts/native-intercept:/home/am57x/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/texinfo-dummy-native:/home/am57x/tisdk/sources/oe-core/scripts:/home/am57x/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/am57x/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/am57x/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/am57x/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/am57x/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/am57x/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/home/am57x/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/am57x/tisdk/sources/oe-core/scripts:/home/am57x/tisdk/sources/meta-browser/scripts:/home/am57x/tisdk/sources/bitbake/bin:/home/am57x/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/am57x/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/am57x/tisdk/sources/oe-core/scripts:/home/am57x/tisdk/sources/meta-browser/scripts:/home/am57x/tisdk/sources/bitbake/bin:/home/am57x/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/am57x"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git.linaro.org/.../binutils-gdb.git /home/am57x/tisdk/downloads/git2/git.linaro.org.toolchain.binutils-gdb.git --progress failed with exit code 128, output:
Cloning into bare repository '/home/am57x/tisdk/downloads/git2/git.linaro.org.toolchain.binutils-gdb.git'...
remote: Counting objects: 1033746, done.
remote: Compressing objects: 100% (165523/165523), done.
error: RPC failed; curl 56 GnuTLS recv error (-9): A TLS packet with unexpected length was received.
fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed
ERROR: binutils-native-linaro-2.27-r2016.10 do_fetch: Fetcher failure for URL: 'git://git.linaro.org/toolchain/binutils-gdb.git;protocol=https;branch=linaro_binutils-2_27-branch'. Unable to fetch URL from any source.
ERROR: binutils-native-linaro-2.27-r2016.10 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/am57x/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/linaro-2.27-r2016.10/temp/log.do_fetch.3793
ERROR: Task (virtual:native:/home/am57x/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/binutils/binutils_linaro-2.27.bb:do_fetch) failed with exit code '1'
but this is ok:
am57x@am57x:~$ git clone git://git.linaro.org/toolchain/binutils-gdb.git;protocol=https;branch=linaro_binutils-2_27-branch