Hello,
Let me confirm AM6526 AVS specification.
VDD_MPU0/1 requirement is defined as 1V+-5% for OPP_NOM, 1.1V+-5% for OPP_OD and 1.22V+-5% for OPP_TURBO in P123 of the datasheet(SPRSP08H)
On the other hand, on the next page, it also says this value is without AVS and AVS value is put on VTM_DEVINFO_VDn.
Then I have a question.
Does power supply for VDD_MPU0/1 has to support AVS?
If using only one OPP, can the power supply voltage be fixed for each used OPP mode, meaning 1V+-5% for OPP_NOM, 1.1V+-5% for OPP_OD and 1.22V+-5% for OPP_TURBO?
Regards,
Oba