Other Parts Discussed in Thread: SYSBIOS
Hello,
To load PDK McASP example image into IPU1 from kenel remote proc module, I added IPC to the example project according to http://software-dl.ti.com/processor-sdk-rtos/esd/docs/latest/rtos/How_to_Guides.html#create-dsp-and-ipu-firmware-using-pdk-drivers-and-ipc-to-load-from-arm-linux-on-am57xx-devices.
There are two tasks in the new project, one is Audio_echo_Task created by mcasp, and another is smain created by ipc. The problems are:
1. According to the remote proc log, there is only one task, which is the one with lower priority, has been scheduled to run.
2. Not any log output from the running task.
3. The task seems not return to run after calling Task_sleep. I guess this maybe caused by the reason that there is not a valiable tick, and I don't have any idea that why the online document ask to "Comment out the entire TICK section". Morover, the result is same even I add the TICK confiuration.
Environment:
DRA762 custom board(NOT a TI EVM)
bios_6_52_00_12 + ipc_3_47_01_00 + pdk_dra7xx_1_0_10
configuration file: /cfs-file/__key/communityserver-discussions-components-files/791/loopback_5F00_m4.cfg