66AK2G12 support,
Please help with these questions:
Does AUD0SC_IN need a pulldown?
The datasheet says ball T1 (UART0_TXD) requires a pulldown if used. Can you confirm, since it's an output?
The datasheet says DDR3_CBQS_P should be pulled LOW if unused. Can you confirm?
The datasheet says DDR3_CBQS_N should be pulled HIGH if unused. Can you confirm? Are these two the right way around?
The datasheet says PORn must transition high a maximum of 2 ms after CVDD/CVDD1. Should that be a minimum rather than maximum? If it's a maximum, it would be nearly impossible to satisfy the SYSOSC_IN requirement of clock being stable for 2 ms prior to PORn being released.
Figures 5-3 and 5-4 do not show the timing of RESET_FULLn, RESETn, LRESETn, LRESETNMIENn and NMIn. Where do we find these details?
Thanks,
Darren