Hi.
We are using TMS320C6655CZHA25 with LM21215AMH-1/NOPB and LM10011SD/NOPB.
I would like to know if the DSP's VCNTL [0: 3] is a signal that can be directly controlled by the user, or a signal that is fixedly sold when the product is manufactured.
If so, which register should I control?
If not, can the user only see the value of VCNTL [0: 3] in the PSC register?
The VCNTLID field value of my board is 0x0FFF0000. Is it OK?
Best Regards