Other Parts Discussed in Thread: TPS62363, INA226
Hello,
I would like to confirm about below.
* Now, we have GPEVM of AM654x. According to schematic of this EVM, VDD_MPUx come from output of TPS62363. And this have following note.
"Default Output voltage is set to 1V"
Actually, when I checked voltage by reading INA226 register value, output voltage indicate 1.0025V.
On the other hand, according following wiki page, TI evaluate EVM using 800MHz as CPU clock.
Now, we have following question.
* According 5.4 Recommended Operating Conditions, there is following description.
– OPP_NOM: 0.9 V – 1.1 V
– OPP_OD: 0.9 V – 1.2 V
– OPP_TURBO: 0.9 V – 1.24 V
On the other hand, according to table 5-2, voltage range is defined as shown below.
Now, TI use 800MHz as CPU clock, so min voltage of VDD_MPU should be bigger than 1.06V.
However, VDD_MPU voltage of EVM is 1.00V in fact.
So, could you please confirm which condition is correct information ?
Best Regards,