Hi,
I previously posted questions about DDR2 measurements which were not okay. We have updated the design to solve the non conformance's. Now I do still see some strange behavior in our signals and was wondering if this is normal behavior or maybe a board or setting problem. (We are running at 266 MHz).
When writing to the memory the signals are looking like this:
and zoomed in:
The signals are measured at the DDR2 device:
S1 (Yellow) -> DQS1_n
S2 (Blue) -> DQS1_p
S4 (Green) -> DQ10
IO_CTRL_x = 0x0000030B
In the last picture where the DQS starts, a glitch or pulse is visible. Is this normal behavior of the signals? And can you give a statement about how the signals are looking?
Please let me know if you need more information. Thank you!
Regards,
F. Veger