Hi!
I'm having a similar problem booting the TMDSIDK574 Development Kit from a micro SD card. It is also a rev. B of the IDK.
The console printouts I received were:
U-Boot SPL 2019.01-ga141f7abfd (Jan 05 2020 - 10:23:38 +0000)
DRA762-GP ES1.0 ABZ package
no pinctrl state for default mode
Card did not respond to voltage select!
Firmware loading failed
Trying to boot from MMC1
no pinctrl state for default mode
Card did not respond to voltage select!
spl: mmc init failed with error: -95
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
I tried with several different microSD cards but with the same results.
We also had a revision 1.0A that boots fine from the same microSD card.
I assume the printed error messages originate from the U-Boot code or the ML, which is on the card, so the MLO must have been read from the card.
Is this a known issue with rev. B of the card?
Is there an alternative way to boot the processor?
Best Regards,
/Anders Axelsson