Hi All
We have implemented a custom board based on GPEVM AM5728 and we are using latest Processor SDK. Only change being TPS6590376 have been replaced with TPS6590378.
Our board keeps rebooting again and again about after 10seconds. Also following logs were observed when booting linux on board:
smps8: Bringing 1010000uV into 1800000-1800000uV
smps8: failed to apply 1800000-1800000uV constraint(-22)
palmas-pmic 48070000.i2c:tps659038@58:tps659038_pmic: failed to register 48070000.i2c:tps659038@58:tps659038_pmic regulator
palmas-pmic: probe of 48070000.i2c:tps659038@58:tps659038_pmic failed with error -22
Additional Findings:
- Measured SMPS8 output is 1.68V instead of 1.8V. (As compared with GPEVM)
- Measured VDDCore output is 1V instead of 1.15V (As compared with GPEVM)
What can be the problem here? Does it need to be fixed in hardware or software?
Thanks & Regards
Amritpreet Singh