Part Number: PROCESSOR-SDK-DRA8X-TDA4X
. I am trying to install the x-86 SDK (06_02_00) on a UBUNTU Linux (18.04 X-64) laptop.
The Install does not happen. I am following the documentation provided.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Devendra,
You have given two different commands in a single attempt without any semi-colon separating them.
So it should be:
chmod +x ti-processor-sdk-linux-automotive-j7-evm-06_02_00.-Linux-x86-Install.bin;
./ti-processor-sdk-linux-automotive-j7-evm-06_02_00.-Linux-x86-Install.bin
Basically they are two separate commands so you can even execute one command
chmod +x ti-processor-sdk-linux-automotive-j7-evm-06_02_00.-Linux-x86-Install.bin
Press enter
Then execute:
./ti-processor-sdk-linux-automotive-j7-evm-06_02_00.-Linux-x86-Install.bin
- Keerthy