Hi,
My customer is planning to replace the compensation resistor on DDR_VTP.
He is planning to change from MELF to chip type.
I found there are some threads discussing about DDR_VTP requirements and understood;
- There is no physical requirements
- 50ohm+/-2% or 49.9ohm+/-1% accuracy can be used.
But it is not clear using bigger power rating (over 20mW) is OK or not.
For example, using 100mW does not harm anything?
https://e2e.ti.com/support/processors/f/791/t/362637
https://e2e.ti.com/support/processors/f/791/t/149668
Thanks and regards,
Koichiro Tashiro