Hi,
I was able to use --float_support=none option when compiling my C code for ARM processor. Thanks for your good advice.
However, the compiled file(.lib) occurs following error when I try to build VisionSDK using the .lib file.
[An error like this: ] *** uses VFP register arguments, *** does not.
I expected this error can be resolved if I use --float_support=none option when compiling C source but not.
Could you give me adveise?
I will attach additional information below:
* Source code for testing
myprintf.h and myprintf.c (Attached to this thread.)
* Commands I entered
../bin/armcl --include_path ../include/ --little_endian --float_support=none myprintf.c
then,
../bin/armar -a myprintf myprintf.obj
and I got myprintf.lib (Attached to this thread).
* Compiler ver.
ti-cgt-arm_18.1.5.LTS
Thanks,
Koji
#include "myprintf.h" void myprintf(int x){ printf("****my_printf_test**** %d \n", x); }