Other Parts Discussed in Thread: AM5748
We returned the original board that failed to boot (see https://e2e.ti.com/support/processors/f/791/t/887175) and received a replacement. The replacement also fails to boot, showing the following error message:
U-Boot SPL 2019.01-g8b90adfb16 (Jul 07 2019 - 01:06:00 +0000)
DRA762-GP ES1.0 ABZ package
Trying to boot from MMC1
no pinctrl state for default mode
no pinctrl state for default mode
Card did not respond to voltage select!
spl: mmc init failed with error: -95
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
I'm using the included Linux SDK SD card. The included Industrial SDK SD card seems to come up and allows board diagnostics to be run.
The board's silkscreen show "REV B", if that is relevant.
Is there anything else I can try, or did I receive two bad kits so far?
Thank you.