Part Number: DRA72XEVM
Hi Experts,
now I am developing the driver for the GMSL sensor.
the system architecture is as below.
below is device tree structure,
&i2c5 {
max9296@48 { compatible = "maxim,max9296"; reg = <0x48>; poc-supply = <&vsys_12v0>; #address-cells = <1>; #size-cells = <0>; ports { #address-cells = <1>; #size-cells = <0>; port@0 { max9296_in0: endpoint { remote-endpoint = <&max9295_out0>; }; }; port@1 { max9296_out0: endpoint { clock-lanes = <0>; data-lanes = <1 2 3 4>; remote-endpoint = <&csi2_phy0>; }; }; }; i2c { #address-cells = <1>; #size-cells = <0>; max9295@40 { compatible = "maxim,max9295"; reg = <0x40>; port { max9295_out0: endpoint { remote-endpoint = <&max9296_in0>; }; }; }; }; };
};
my question are as follow:
1. does the device tree is correct?
2. does TI have the sample driver code for GMSL? is it possible provide us to reference?
3. have any suggestion to implement this driver? do we need to implement driver for MAX9295 and MAX9296?
Thanks.