Hi,
SOC : DRA746
SDK : Vision SDK 3.04
Display resolution : 800*480
Board type : Custom board
For our custom board, for carplay playback, we have below gstreamer pipeline to play the h264 stream from Iphone on the display
appsrc | ducatidecoder | waylandsink
Sometimes, we see the surface creation is not happening in the gstreamer within gstwaylandsink.
Attached are complete working and non-working case gstreamer debug logs.
Please check and help on this.
/cfs-file/__key/communityserver-discussions-components-files/791/non_2D00_working.txt
/cfs-file/__key/communityserver-discussions-components-files/791/working.txt
For non-working case : No further gstreamer logs are seen after below lines
0:00:11.242008833 2287 0x238320 DEBUG waylandsink gstwaylandsink.c:478:gst_wayland_sink_get_caps:<videoSink> display caps: video/x-raw, format=(string){ BGRA, BGRx, RGB16, YUV9, Y41B, I420, Y42B, v308, NV12, NV16, YUY2, UYVY }, width=(int)[ 1, 2147483647 ], height=(int)[ 1, 2147483647 ], framerate=(fraction)[ 0/1, 2147483647/1 ]
0:00:11.242129986 2287 0x238320 DEBUG waylandsink gstwaylandsink.c:523:gst_wayland_sink_set_caps:<videoSink> set caps video/x-raw, format=(string)NV12, width=(int)896, height=(int)576, framerate=(fraction)30/1, drm_mem=(boolean)true
0:00:11.242191155 2287 0x238320 DEBUG waylandsink gstwaylandsink.c:498:wait_authentication:<videoSink> Before wait aunthenticated value is 1 :
0:00:11.242224028 2287 0x238320 DEBUG waylandsink gstwaylandsink.c:503:wait_authentication:<videoSink> After wait aunthenticated value is 1 :
Best Regards,
Pradeep G